<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: unable to unlock S32K148 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1268591#M60410</link>
    <description>&lt;P&gt;I've found a solution&lt;BR /&gt;resolvent&lt;BR /&gt;1) If the hardware circuit board supports modification, the VDD of the chip can be connected to On Pin1 of J_link&lt;BR /&gt;2) If the hardware circuit board does not support changes, you can also change the Pin1 and Pin2 short circuit of J_link&lt;BR /&gt;Special notes&lt;BR /&gt;1) The problem of unable to download the code may appear on all MCU, which will prompt that the chip core cannot be found&lt;BR /&gt;2) Pin1 and Pin2 have been short circuited in the new version of j-link (for example, v8.3), so the above problems will not occur&lt;BR /&gt;3) Recommendation J_ Link to connect with the target board, please connect to RST signal, that is: VDD, VSS, GND, swdio, swclk, RST signal&lt;/P&gt;</description>
    <pubDate>Tue, 27 Apr 2021 06:39:50 GMT</pubDate>
    <dc:creator>ljmljmljm</dc:creator>
    <dc:date>2021-04-27T06:39:50Z</dc:date>
    <item>
      <title>unable to unlock S32K148</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1264216#M60264</link>
      <description>&lt;P&gt;Download always show error “Could not find core in Coresight setup”&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="捕获.PNG" style="width: 929px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142632iA57EA38732327593/image-size/large?v=v2&amp;amp;px=999" role="button" title="捕获.PNG" alt="捕获.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="捕获1.PNG" style="width: 996px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142633iEF86813115490E49/image-size/large?v=v2&amp;amp;px=999" role="button" title="捕获1.PNG" alt="捕获1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="捕获3.PNG" style="width: 848px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142634i66C0F427E5B2F6C0/image-size/large?v=v2&amp;amp;px=999" role="button" title="捕获3.PNG" alt="捕获3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 08:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1264216#M60264</guid>
      <dc:creator>ljmljmljm</dc:creator>
      <dc:date>2021-04-19T08:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: unable to unlock S32K148</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1265023#M60290</link>
      <description>&lt;P&gt;Hi ljmljmljm,&lt;/P&gt;
&lt;P&gt;Please refer:&amp;nbsp;&lt;A href="https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&amp;amp;mid=2247484245&amp;amp;idx=1&amp;amp;sn=3561b3bada7ab46acb3747ed9837769c&amp;amp;chksm=e91247d3de65cec51fb4b88556593da08b5e8613c2f487abbe593a7879cecdfbbe598b51ce11&amp;amp;scene=21#wechat_redirect" target="_self"&gt;S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 09:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1265023#M60290</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-04-20T09:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: unable to unlock S32K148</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1268591#M60410</link>
      <description>&lt;P&gt;I've found a solution&lt;BR /&gt;resolvent&lt;BR /&gt;1) If the hardware circuit board supports modification, the VDD of the chip can be connected to On Pin1 of J_link&lt;BR /&gt;2) If the hardware circuit board does not support changes, you can also change the Pin1 and Pin2 short circuit of J_link&lt;BR /&gt;Special notes&lt;BR /&gt;1) The problem of unable to download the code may appear on all MCU, which will prompt that the chip core cannot be found&lt;BR /&gt;2) Pin1 and Pin2 have been short circuited in the new version of j-link (for example, v8.3), so the above problems will not occur&lt;BR /&gt;3) Recommendation J_ Link to connect with the target board, please connect to RST signal, that is: VDD, VSS, GND, swdio, swclk, RST signal&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 06:39:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/unable-to-unlock-S32K148/m-p/1268591#M60410</guid>
      <dc:creator>ljmljmljm</dc:creator>
      <dc:date>2021-04-27T06:39:50Z</dc:date>
    </item>
  </channel>
</rss>