<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C inputs 5v tolerant? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242277#M6040</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not sure that if the back-biased protection diodes stay connected to 3.3V Kinetis pins when you configure them to I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you tie pull-up resistors to 3.3V, it should work with no risk to any component tied to I2C. Inputs of 3.3V devices will not hold any chance to be overloaded, and inputs of 5V devices will recognize the 3.3V on SDA and SCL lines as high-level. I have worked on many projects where I connected 3.3V outputs to 5V inputs, and logic levels were always recongized correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this is my suggestion: use pull-up resistors tied to 3.3V if there is any 3.3V device connected to I2C bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Nov 2013 15:20:47 GMT</pubDate>
    <dc:creator>quevedo</dc:creator>
    <dc:date>2013-11-05T15:20:47Z</dc:date>
    <item>
      <title>I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242267#M6030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the I2C interface 5v tolerant?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 13:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242267#M6030</guid>
      <dc:creator>matthewdoveton</dc:creator>
      <dc:date>2013-10-28T13:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242268#M6031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matthew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working on my FRDM-KL25Z at 5v and it's working perfectly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hector&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 15:57:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242268#M6031</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-10-28T15:57:53Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242269#M6032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Hector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm. Does the open collector input stay at 5v or is it clamped to Vdd?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 16:14:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242269#M6032</guid>
      <dc:creator>matthewdoveton</dc:creator>
      <dc:date>2013-10-28T16:14:08Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242270#M6033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recommend you to check this thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/327309"&gt;Re: Kinetis 5V I2C interface&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 16:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242270#M6033</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-10-28T16:41:16Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242271#M6034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Matthew&lt;/P&gt;&lt;P&gt;You need to use pull-up resistor to connect 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2013 01:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242271#M6034</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-10-29T01:20:39Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242272#M6035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you post a scope shot?&amp;nbsp; There is certainly some 'confusion' around as to whether the Kinetis I2C pins, in 'open collector I/O mode', get clamped by a 'parasitic' high-side (undriven!) transistor.&amp;nbsp; There is a statement that pins are 5V tolerant ONLY in 'input only' mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2013 11:40:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242272#M6035</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2013-10-29T11:40:38Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242273#M6036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at that thread, still never fully answered the question.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Oct 2013 11:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242273#M6036</guid>
      <dc:creator>matthewdoveton</dc:creator>
      <dc:date>2013-10-30T11:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242274#M6037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I do know that pull-ups would be required. What I am really unsure of is whether the inputs would be pulled up to 5v or about 3.6v. Do these inputs have overvoltage protection that will prevent the inputs from maintaining 5v? This seems unclear to me. I have scoured the datasheets but still unsure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Oct 2013 11:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242274#M6037</guid>
      <dc:creator>matthewdoveton</dc:creator>
      <dc:date>2013-10-30T11:16:10Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242275#M6038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no 'input protection' diode to VDD, BUT my expectation, given the item in the other thread by Derek Snell, is that the 'back biased diode' inherent in the pull-up transistor of the push-pull output structure is 'still there' even in open-collector mode (just never made active!), so THAT diode will clamp a bidirectional-I/O-mode pin to the rail.&amp;nbsp; A proof picture would be nice -- but I don't have any 5V I2C busses.&amp;nbsp; One other option for you would be an I2C repeater like PCA9509 or PCA9515...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Oct 2013 22:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242275#M6038</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2013-10-30T22:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242276#M6039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well I'm going to add a level translator to my prototype in case its needed. I will investigate and post the results back here. This will be in approx. 2 weeks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2013 10:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242276#M6039</guid>
      <dc:creator>matthewdoveton</dc:creator>
      <dc:date>2013-10-31T10:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242277#M6040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not sure that if the back-biased protection diodes stay connected to 3.3V Kinetis pins when you configure them to I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you tie pull-up resistors to 3.3V, it should work with no risk to any component tied to I2C. Inputs of 3.3V devices will not hold any chance to be overloaded, and inputs of 5V devices will recognize the 3.3V on SDA and SCL lines as high-level. I have worked on many projects where I connected 3.3V outputs to 5V inputs, and logic levels were always recongized correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this is my suggestion: use pull-up resistors tied to 3.3V if there is any 3.3V device connected to I2C bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2013 15:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242277#M6040</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2013-11-05T15:20:47Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242278#M6041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All I can say about that is check your Vih(min) spec!&amp;nbsp; Many 'modern' CMOS parts stick to the 0.7*Vcc requirement, which at 5V+5% is 3.675V -- can be hard to hit, even driving against 'diode clamps' to a 3.3V-5% power rail -- needs 0.54V over-rail-drive (with NO resulting noise margin!).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2013 19:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242278#M6041</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2013-11-05T19:26:00Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242279#M6042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe we should ask first why the question was posted in the first place. We are supposing that Matthew intends to connect some 5V I2C device on the I2C bus of a Kinetis powered with 3.3V. I woule like to know what he intends to connect to the bus, i.e., the part number. Maybe there is a 3.3V version for the same function. Even if he has to use the 5V part, we could check data sheet and see if Vih(min) specs are met.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Nov 2013 12:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242279#M6042</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2013-11-10T12:36:54Z</dc:date>
    </item>
    <item>
      <title>Re: I2C inputs 5v tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242280#M6043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've measured SDA and SCL high voltage at 4.0V and 4.1V when pulled up to 5V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Mar 2014 12:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-inputs-5v-tolerant/m-p/242280#M6043</guid>
      <dc:creator>OliverSedlacek</dc:creator>
      <dc:date>2014-03-24T12:30:46Z</dc:date>
    </item>
  </channel>
</rss>