<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: does the Kinetis K81 USB suspend is available when connected with Android device?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1267201#M60358</link>
    <description>&lt;P&gt;it looks like &lt;SPAN&gt;USB autosuspend&lt;/SPAN&gt; did not enabled on the Android device?&lt;/P&gt;&lt;P&gt;thank you for your response&lt;/P&gt;</description>
    <pubDate>Fri, 23 Apr 2021 09:14:33 GMT</pubDate>
    <dc:creator>robinliao</dc:creator>
    <dc:date>2021-04-23T09:14:33Z</dc:date>
    <item>
      <title>does the Kinetis K81 USB suspend is available when connected with Android device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1262721#M60215</link>
      <description>&lt;P&gt;Hello NXP&lt;/P&gt;&lt;P&gt;Is the usb pause mode available when connected to an Android phone/tablet?&lt;/P&gt;&lt;P&gt;I have implemented the USB suspend function on our device and it works fine&lt;/P&gt;&lt;P&gt;my usb devices can be suspended/resume when connected to the host PC&lt;/P&gt;&lt;P&gt;but when I connect to the Android phone, the usb device is always running, and will not enter the USB suspend state&lt;/P&gt;&lt;P&gt;How to configure the usb library to support usb suspend on Android devices? Or is this problem based on the Android configuration?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 09:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1262721#M60215</guid>
      <dc:creator>robinliao</dc:creator>
      <dc:date>2021-04-15T09:41:48Z</dc:date>
    </item>
    <item>
      <title>Re: does the Kinetis K81 USB suspend is available when connected with Android device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1265325#M60296</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;
&lt;P&gt;We do not have specific configuration for Android devices in our USB stack, therefore, I think the problem could be on the Android side, maybe there is a some driver missing.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 18:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1265325#M60296</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-04-20T18:10:49Z</dc:date>
    </item>
    <item>
      <title>Re: does the Kinetis K81 USB suspend is available when connected with Android device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1267201#M60358</link>
      <description>&lt;P&gt;it looks like &lt;SPAN&gt;USB autosuspend&lt;/SPAN&gt; did not enabled on the Android device?&lt;/P&gt;&lt;P&gt;thank you for your response&lt;/P&gt;</description>
      <pubDate>Fri, 23 Apr 2021 09:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-the-Kinetis-K81-USB-suspend-is-available-when-connected/m-p/1267201#M60358</guid>
      <dc:creator>robinliao</dc:creator>
      <dc:date>2021-04-23T09:14:33Z</dc:date>
    </item>
  </channel>
</rss>