<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TRGMUX Port Pin Trigger</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1265958#M60309</link>
    <description>&lt;P&gt;Hi Felipe,&lt;/P&gt;&lt;P&gt;I just made simple program with few lines of code to demonstrate this, together with scope screenshots, to attach all together here.&lt;/P&gt;&lt;P&gt;But, everything is working fine as it should. Only port pin that is triggering FlexIO timers start / stop is one pin with&amp;nbsp; IRQC 13. Other pins with IRQC 0 doesn't disturb FlexIO timers on any way. So everything is OK with device, problem is somewhere else in my code.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
    <pubDate>Wed, 21 Apr 2021 15:27:57 GMT</pubDate>
    <dc:creator>jh0</dc:creator>
    <dc:date>2021-04-21T15:27:57Z</dc:date>
    <item>
      <title>TRGMUX Port Pin Trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1261329#M60181</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to start/stop FlexIO timers with one (non FlexIO) port pin. When pin goes high, timers are started, and when pin goes low, timers are stopped.&lt;/P&gt;&lt;P&gt;I configured (port A pin 1) with PORT PCR values MUX 1 (GPIO) and IRQC 13 (&lt;EM&gt;Enable active high trigger output, flag is disabled. [The trigger output goes to the trigger mux, which allows pins to trigger other peripherals (configurable polarity; &lt;FONT color="#000000"&gt;1 pin per port&lt;/FONT&gt;; if multiple pins are configured, then they are ORed together to create the trigger)].&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I configured TRGMUX_FLEXIO0 with SEL0 value 0x2A Port A Pin Trigger is selected.&lt;/P&gt;&lt;P&gt;Also configured FlexOI timers and everything is working fine, as expected.&lt;/P&gt;&lt;P&gt;But when I change state of other pin on port A, this have influence on trigger, and I don't understand why, because for all other pins on the same port A, IRQC value in PCR is zero. How I can isolate trigger to just one port pin?&lt;/P&gt;&lt;P&gt;Device is K32L2A31.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 13:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1261329#M60181</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2021-04-13T13:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Port Pin Trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1265240#M60294</link>
      <description>&lt;P&gt;Hi Josip,&lt;/P&gt;
&lt;P&gt;Could you please share the code you are using to configure TRGMUX? I would like to investigate this in more detail.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 14:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1265240#M60294</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-04-20T14:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Port Pin Trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1265958#M60309</link>
      <description>&lt;P&gt;Hi Felipe,&lt;/P&gt;&lt;P&gt;I just made simple program with few lines of code to demonstrate this, together with scope screenshots, to attach all together here.&lt;/P&gt;&lt;P&gt;But, everything is working fine as it should. Only port pin that is triggering FlexIO timers start / stop is one pin with&amp;nbsp; IRQC 13. Other pins with IRQC 0 doesn't disturb FlexIO timers on any way. So everything is OK with device, problem is somewhere else in my code.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 15:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TRGMUX-Port-Pin-Trigger/m-p/1265958#M60309</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2021-04-21T15:27:57Z</dc:date>
    </item>
  </channel>
</rss>