<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL27Z128V memory Map</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1265139#M60292</link>
    <description>&lt;P&gt;For the parts that do not have dedicated USB memory, the normal system memory is used.&lt;BR /&gt;The start of that buffer must be aligned on a 512 byte boundary.&lt;/P&gt;&lt;P&gt;The buffer as a whole must not cross the high/low memory split.&lt;BR /&gt;Some parts don't care about the split, many do.&lt;BR /&gt;Use the linker to place it in a specific section at a specific location if needed.&lt;BR /&gt;&lt;BR /&gt;Example for GCC:&lt;/P&gt;&lt;P&gt;#ifndef ENDPOINTS_USED&lt;BR /&gt;#define ENDPOINTS_USED (3U) /* Including the Control Endpoint */&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#if( ENDPOINTS_USED &amp;gt; 16U )&lt;BR /&gt;#error More than 16 End Points is not allowed.&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#define BDT_PER_EP (4U) /* 4 = (TX Odd/Even) + (RX Odd/Even) */&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Every endpoint direction requires two 8-byte Buffer Descriptor (BD)&lt;BR /&gt;* entries. This part is Little Endian.&lt;BR /&gt;*/&lt;BR /&gt;typedef struct BDT&lt;BR /&gt;{&lt;BR /&gt;uint8_t bdctl_u8; /* Buffer Descriptor Control BD[ 0: 7] */&lt;BR /&gt;uint8_t rsvd_u8; /* Reserved: BD[ 8:15] */&lt;BR /&gt;uint16_t byte_count_u16; /* Byte Count. Only ten bits are used for the count. BD[16:32] */&lt;BR /&gt;uint8_t *addr_ptr_u8; /* Address */&lt;BR /&gt;} BDT;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* There are:&lt;BR /&gt;* * 16 bidirectionnal end points -&amp;gt; 16 Rx, 16 Tx end points,&lt;BR /&gt;* * and there are ODD and EVEN buffer, for ping/ponging, -&amp;gt; 64 bdt's.&lt;BR /&gt;*/&lt;BR /&gt;static BDT bdt[( ENDPOINTS_USED * BDT_PER_EP ) ] __attribute__( ( __aligned__( 512U ) ) );&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Apr 2021 12:29:54 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2021-04-20T12:29:54Z</dc:date>
    <item>
      <title>KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1263849#M60251</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are trying to run a USB code that was written for the KL27Z64V on the KL27Z128V and we are getting a hard fault since the memory map for both the controllers doesn't match. Hence we are looking for the memory map for the USB RAM for the KL27Z128V.&lt;/P&gt;&lt;P&gt;We already have the same for the KL27Z64V from Page 27 of this link: &lt;A href="https://www.nxp.com/docs/en/data-sheet/KL27P64M48SF2.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/KL27P64M48SF2.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The USB RAM memory location is 0x400F_E000 for the KL27Z64V but what is it for the KL27Z128V is what we want to understand. Is there a document that you can direct us to?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Neel.&lt;/P&gt;</description>
      <pubDate>Sat, 17 Apr 2021 07:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1263849#M60251</guid>
      <dc:creator>ND2</dc:creator>
      <dc:date>2021-04-17T07:40:20Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1263947#M60255</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;neelshah，&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; You have refer to the wrong document, please refer to this document:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/KL27P64M48SF6RM.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/KL27P64M48SF6RM.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This is for&amp;nbsp;&lt;SPAN&gt;KL27Z128V,&amp;nbsp;KL27Z64V and&amp;nbsp;KL27Z128V is not the same.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So, please check the correct document first.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you still have issues, just kindly let me know.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 02:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1263947#M60255</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-04-19T02:53:57Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1263981#M60257</link>
      <description>&lt;P&gt;Dear Kerry,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;We did look at this link too during our research. We loved at page 543-545 but can’t seem to find the starting address of the USB RAM.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Can you please point it out for us?&lt;/P&gt;&lt;P&gt;Neel.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 04:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1263981#M60257</guid>
      <dc:creator>ND2</dc:creator>
      <dc:date>2021-04-19T04:31:23Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1264004#M60258</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/139124" target="_self"&gt;neelshah&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;KL27Z64V has the specific USB RAM, but KL27Z128V doesn't have the specific USB RAM, you may need to use the chip normal SRAM.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 05:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1264004#M60258</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-04-19T05:39:43Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1265139#M60292</link>
      <description>&lt;P&gt;For the parts that do not have dedicated USB memory, the normal system memory is used.&lt;BR /&gt;The start of that buffer must be aligned on a 512 byte boundary.&lt;/P&gt;&lt;P&gt;The buffer as a whole must not cross the high/low memory split.&lt;BR /&gt;Some parts don't care about the split, many do.&lt;BR /&gt;Use the linker to place it in a specific section at a specific location if needed.&lt;BR /&gt;&lt;BR /&gt;Example for GCC:&lt;/P&gt;&lt;P&gt;#ifndef ENDPOINTS_USED&lt;BR /&gt;#define ENDPOINTS_USED (3U) /* Including the Control Endpoint */&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#if( ENDPOINTS_USED &amp;gt; 16U )&lt;BR /&gt;#error More than 16 End Points is not allowed.&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#define BDT_PER_EP (4U) /* 4 = (TX Odd/Even) + (RX Odd/Even) */&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Every endpoint direction requires two 8-byte Buffer Descriptor (BD)&lt;BR /&gt;* entries. This part is Little Endian.&lt;BR /&gt;*/&lt;BR /&gt;typedef struct BDT&lt;BR /&gt;{&lt;BR /&gt;uint8_t bdctl_u8; /* Buffer Descriptor Control BD[ 0: 7] */&lt;BR /&gt;uint8_t rsvd_u8; /* Reserved: BD[ 8:15] */&lt;BR /&gt;uint16_t byte_count_u16; /* Byte Count. Only ten bits are used for the count. BD[16:32] */&lt;BR /&gt;uint8_t *addr_ptr_u8; /* Address */&lt;BR /&gt;} BDT;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* There are:&lt;BR /&gt;* * 16 bidirectionnal end points -&amp;gt; 16 Rx, 16 Tx end points,&lt;BR /&gt;* * and there are ODD and EVEN buffer, for ping/ponging, -&amp;gt; 64 bdt's.&lt;BR /&gt;*/&lt;BR /&gt;static BDT bdt[( ENDPOINTS_USED * BDT_PER_EP ) ] __attribute__( ( __aligned__( 512U ) ) );&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 12:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1265139#M60292</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-04-20T12:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1267634#M60381</link>
      <description>&lt;P&gt;The challenge is with the USB RAM address. The SDK is based on the KL27Z64V but I have a freedom board which is based on the KL27Z128V. Not sure what should be the USB_RAM address.&lt;/P&gt;&lt;P&gt;Can you please advice?&lt;/P&gt;</description>
      <pubDate>Sun, 25 Apr 2021 07:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1267634#M60381</guid>
      <dc:creator>ND2</dc:creator>
      <dc:date>2021-04-25T07:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z128V memory Map</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1267750#M60390</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;&lt;A id="link_37" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/139124" target="_self"&gt;neelshah&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; In fact, you have refered to the wrong SDK code, normally, to the KL27Z128 SDK code, you can download it directly, and it is based on the KL43 FRDM, please download the correct core again, you will know the detail USB_RAM usage:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;&lt;A href="https://mcuxpresso.nxp.com/" target="_blank"&gt;https://mcuxpresso.nxp.com/&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1619404923192.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/143173i91A18B41B0D28AAC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1619404923192.png" alt="kerryzhou_0-1619404923192.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kerryzhou_0-1619404923192.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;After you download it, you may find the project is based on the KL43 directly, but don't worry, you can change the related project drivers and startup files in this folder:&lt;/P&gt;
&lt;P&gt;SDK_2.8.0_MKL27Z128xxx4\devices\MKL27Z4&lt;/P&gt;
&lt;P&gt;All the drivers are listed. The USB drivers is the same stack.&lt;/P&gt;
&lt;P&gt;Please try it on your side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 02:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z128V-memory-Map/m-p/1267750#M60390</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-04-26T02:44:09Z</dc:date>
    </item>
  </channel>
</rss>