<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RX-TX Pokayoke in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/RX-TX-Pokayoke/m-p/242236#M6021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sometimes, RX-TX transceiver interconnections aren’t well defined about who is the module that transmits or receives. This is due to lags in design requirements or information missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Proposed strategy consists in including a couple of series resistors in the TX and RX nets as shunts. These resistors might also work also as current limiters. 0603 size was used for this strategy.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42586i0BB4BC16ACF79D7B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The resistor shunts will provide a platform to intercross RX to TX connections by rotating these resistors 90 degrees in a rework.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42588iF1C3DA8F603746AB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this reason one of these resistors should rotate 180 degrees in layout, and both resistors should be placed one besides the other, maintaining same air gap between resistors’ pads, therefore, preserving its schematic connections.&lt;/P&gt;&lt;P align="center" style="text-align: center;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42589i8B14AFB5B20C5CAF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAD should look similar to this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42633iBA48B47124570B6D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a final result, in case of misconnection, a quick rework consisting in 90 degrees resistors’ rotation will fix the issue.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42509iAA73D06DADCBA866/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Feb 2014 16:35:47 GMT</pubDate>
    <dc:creator>jrdelrey</dc:creator>
    <dc:date>2014-02-18T16:35:47Z</dc:date>
    <item>
      <title>RX-TX Pokayoke</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/RX-TX-Pokayoke/m-p/242236#M6021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sometimes, RX-TX transceiver interconnections aren’t well defined about who is the module that transmits or receives. This is due to lags in design requirements or information missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Proposed strategy consists in including a couple of series resistors in the TX and RX nets as shunts. These resistors might also work also as current limiters. 0603 size was used for this strategy.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42586i0BB4BC16ACF79D7B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The resistor shunts will provide a platform to intercross RX to TX connections by rotating these resistors 90 degrees in a rework.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42588iF1C3DA8F603746AB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this reason one of these resistors should rotate 180 degrees in layout, and both resistors should be placed one besides the other, maintaining same air gap between resistors’ pads, therefore, preserving its schematic connections.&lt;/P&gt;&lt;P align="center" style="text-align: center;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42589i8B14AFB5B20C5CAF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAD should look similar to this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42633iBA48B47124570B6D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a final result, in case of misconnection, a quick rework consisting in 90 degrees resistors’ rotation will fix the issue.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42509iAA73D06DADCBA866/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 16:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/RX-TX-Pokayoke/m-p/242236#M6021</guid>
      <dc:creator>jrdelrey</dc:creator>
      <dc:date>2014-02-18T16:35:47Z</dc:date>
    </item>
  </channel>
</rss>