<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Connecting to FRDM-K64F Board in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connecting-to-FRDM-K64F-Board/m-p/1261591#M60196</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The bootloader is not matching your firmware. You now need an external debugger(jlink) to update the bootloader. Follow the attachment.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 02:03:22 GMT</pubDate>
    <dc:creator>nxf56274</dc:creator>
    <dc:date>2021-04-14T02:03:22Z</dc:date>
    <item>
      <title>Connecting to FRDM-K64F Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connecting-to-FRDM-K64F-Board/m-p/1261523#M60193</link>
      <description>&lt;P&gt;Hello, I am trying to connect to my FRDM-K64F Board which has a FRDM-STBC-AGM01 Board attached to it. My goal is to use the Freedom Sensor Toolbox (CE)(v2.5.0) to run an Out of the Box Demo.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Originally, The device would show up on my computer as MED in the file explorer. But, would eventually show a fail text with TIMEOUT inside. The Freedom software only ever shows "waiting for a board to be connected..."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed the steps at this link to make sure the device was setup correctly: &lt;A href="https://www.nxp.com/design/software/development-software/sensor-toolbox-sensor-development-ecosystem/freedom-sensor-toolbox-community-edition-sensor-evaluation-and-visualization-software:SENSOR-TOOLBOX-CE?&amp;amp;tab=In-Depth_Tab" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/software/development-software/sensor-toolbox-sensor-development-ecosystem/freedom-sensor-toolbox-community-edition-sensor-evaluation-and-visualization-software:SENSOR-TOOLBOX-CE?&amp;amp;tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw that the device can become corrupted when plugging into a Windows 10 device which is what I am trying to use. So, I went through the steps to update the OpenSDA at this link using the dropdown box: &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA#FRDM-K64F" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA#FRDM-K64F&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There I downloaded this Binary "DAPLink rev0244 OpenSDA v2.2 Bootloader" and proceeded with the update instructions. The drive showed up as BOOTLOADER and I pasted the downloaded binary inside. (Note: The BOOTLOADER drive did not stay up for very long inside my file explorer.). After this though when I plugged the USB back in I see no sign of connection in the file explorer or on the computer and no blinking lights on the board. I attempted to do the Bootloader steps again and the BOOTLOADER Drive would always show back up but I could still never see any sign of connection afterwards. The software also would continue to say "waiting for a board to be connected..." Is there a crucial step that I am missing to properly connect this device to my computer?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 21:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connecting-to-FRDM-K64F-Board/m-p/1261523#M60193</guid>
      <dc:creator>Bas0037</dc:creator>
      <dc:date>2021-04-13T21:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting to FRDM-K64F Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connecting-to-FRDM-K64F-Board/m-p/1261591#M60196</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The bootloader is not matching your firmware. You now need an external debugger(jlink) to update the bootloader. Follow the attachment.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 02:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connecting-to-FRDM-K64F-Board/m-p/1261591#M60196</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-04-14T02:03:22Z</dc:date>
    </item>
  </channel>
</rss>