<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KE18F ECC 1-Bit Correction and 3-Bit Detection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-ECC-1-Bit-Correction-and-3-Bit-Detection/m-p/1259555#M60137</link>
    <description>&lt;P&gt;Hi sean,&lt;/P&gt;
&lt;P&gt;ECC function can't be modify or close in KE18F. ECC function is not like CRC. There bit error are sure can be found.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Fri, 09 Apr 2021 09:35:30 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-04-09T09:35:30Z</dc:date>
    <item>
      <title>KE18F ECC 1-Bit Correction and 3-Bit Detection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-ECC-1-Bit-Correction-and-3-Bit-Detection/m-p/1259119#M60128</link>
      <description>I am looking for some documentation about whether or not the KE18F automatically fixes all 1-Bit ECC errors. The manual does not say anything about correcting the 1-Bit errors, but AN5332 says, "detection and correction of up to a 1-bit error". If the KE18F is fixing these 1-bit errors, is there a way to stop it from correcting and only report them? There is a bit of concern about 3-Bit errors looking like 1-Bit errors, and would like for it not to try and fix anything in that instance. Just report it.</description>
      <pubDate>Thu, 08 Apr 2021 20:35:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-ECC-1-Bit-Correction-and-3-Bit-Detection/m-p/1259119#M60128</guid>
      <dc:creator>sean_dvorscak</dc:creator>
      <dc:date>2021-04-08T20:35:13Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F ECC 1-Bit Correction and 3-Bit Detection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-ECC-1-Bit-Correction-and-3-Bit-Detection/m-p/1259555#M60137</link>
      <description>&lt;P&gt;Hi sean,&lt;/P&gt;
&lt;P&gt;ECC function can't be modify or close in KE18F. ECC function is not like CRC. There bit error are sure can be found.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 09:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-ECC-1-Bit-Correction-and-3-Bit-Detection/m-p/1259555#M60137</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-04-09T09:35:30Z</dc:date>
    </item>
  </channel>
</rss>