<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFTM Counter</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Counter/m-p/1255009#M60051</link>
    <description>&lt;P&gt;The KE1xZ microcontroller has 3 Flexible Timer modules, 1 with 8 channels and 2 others, with 4 channels. I intend to configure one of the modules to make Capture signal and another module to generate 4 different PWM signals. I ask if the 16-bit counter of the FTM modules are independent for the various modules or if it is the same counter that serves all FTM?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Wed, 31 Mar 2021 14:22:10 GMT</pubDate>
    <dc:creator>Jmir</dc:creator>
    <dc:date>2021-03-31T14:22:10Z</dc:date>
    <item>
      <title>FTM Counter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Counter/m-p/1255009#M60051</link>
      <description>&lt;P&gt;The KE1xZ microcontroller has 3 Flexible Timer modules, 1 with 8 channels and 2 others, with 4 channels. I intend to configure one of the modules to make Capture signal and another module to generate 4 different PWM signals. I ask if the 16-bit counter of the FTM modules are independent for the various modules or if it is the same counter that serves all FTM?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 14:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Counter/m-p/1255009#M60051</guid>
      <dc:creator>Jmir</dc:creator>
      <dc:date>2021-03-31T14:22:10Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Counter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Counter/m-p/1255072#M60055</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184341"&gt;@Jmir&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&lt;/P&gt;
&lt;P&gt;In this case each FTM as an independient counter, called FTMx_CNT, where the x stands for the number of the FTM module, for example FTM0_CNT, FTM1_CNT, FTM2_CNT.&lt;/P&gt;
&lt;P&gt;Additionally, You can take a look at our SDK examples for FTM from our MCUxpresso SDK!&amp;nbsp; and if you like, you can&amp;nbsp; use our Config tools&amp;nbsp; to generate initialization code for the FTM.&lt;/P&gt;
&lt;P&gt;I hope this helps.&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 16:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Counter/m-p/1255072#M60055</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2021-03-31T16:22:15Z</dc:date>
    </item>
  </channel>
</rss>