<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Memory to SPI (Peripheral) via DMA code snippet for KM34Z128 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Memory-to-SPI-Peripheral-via-DMA-code-snippet-for-KM34Z128/m-p/1253350#M60025</link>
    <description>Hi Triggered by an external interrupt, I would like to send 64 bytes buffer (array) through SPI Bus using DMA, can I have any example for the same Target MCU : MKM34Z128 (50 Mhz) Thank you, Paddy</description>
    <pubDate>Mon, 29 Mar 2021 05:58:46 GMT</pubDate>
    <dc:creator>phamsa</dc:creator>
    <dc:date>2021-03-29T05:58:46Z</dc:date>
    <item>
      <title>Memory to SPI (Peripheral) via DMA code snippet for KM34Z128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Memory-to-SPI-Peripheral-via-DMA-code-snippet-for-KM34Z128/m-p/1253350#M60025</link>
      <description>Hi Triggered by an external interrupt, I would like to send 64 bytes buffer (array) through SPI Bus using DMA, can I have any example for the same Target MCU : MKM34Z128 (50 Mhz) Thank you, Paddy</description>
      <pubDate>Mon, 29 Mar 2021 05:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Memory-to-SPI-Peripheral-via-DMA-code-snippet-for-KM34Z128/m-p/1253350#M60025</guid>
      <dc:creator>phamsa</dc:creator>
      <dc:date>2021-03-29T05:58:46Z</dc:date>
    </item>
    <item>
      <title>Re: Memory to SPI (Peripheral) via DMA code snippet for KM34Z128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Memory-to-SPI-Peripheral-via-DMA-code-snippet-for-KM34Z128/m-p/1255268#M60056</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/8695"&gt;@phamsa&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, this specific example that you mention is not available but in the SDK for the KM34 (75MHz) you can find an example using an SPI DMA transfer using a software trigger. The SDK is not straight compatible with the KM34 (50 MHz) but the SPI and DMA should be the same.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 21:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Memory-to-SPI-Peripheral-via-DMA-code-snippet-for-KM34Z128/m-p/1255268#M60056</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-03-31T21:39:01Z</dc:date>
    </item>
  </channel>
</rss>