<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Realistically priced debugger/programmer for low volume users</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Realistically-priced-debugger-programmer-for-low-volume-users/m-p/1252602#M60010</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/128557"&gt;@richardfritz&lt;/a&gt; ,&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Even NXP has one for LPC ARM chips...for $25...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Not only LPC, but as well Kinetis and i.MX RT.&lt;/P&gt;&lt;P&gt;I use the LPC-Link2 (or embedded circuit of it on the boards) for all kind of the Kinetis devices (Kinetis-K, Kinetis-L for example) including the i.MX RT parts with the MCUXpresso IDE. You might be confused by the naming of the probe (agreed, probably for historical reasons), but it is *not* only for LPC, but as well for Kinetis and i.MX RT parts. Have a look at &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-link2:OM13054" target="_blank"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-link2:OM13054&lt;/A&gt; which lists the supported devices.&lt;/P&gt;&lt;P&gt;The LPC-Link2 is priced $20, but since some time there is the MCU-Link (notice the name) which is the successor of the LPC-Link2 and costs only $10 (see &lt;A href="https://www.nxp.com/design/development-boards/lpcxpresso-boards/mcu-link-debug-probe:MCU-LINK" target="_blank"&gt;https://www.nxp.com/design/development-boards/lpcxpresso-boards/mcu-link-debug-probe:MCU-LINK&lt;/A&gt; or my articles &lt;A href="https://mcuoneclipse.com/2020/11/29/new-mcu-link-debug-probe-from-nxp/" target="_blank"&gt;https://mcuoneclipse.com/2020/11/29/new-mcu-link-debug-probe-from-nxp/&lt;/A&gt; or &lt;A href="https://mcuoneclipse.com/tag/mcu-link/" target="_blank"&gt;https://mcuoneclipse.com/tag/mcu-link/&lt;/A&gt; ).&lt;/P&gt;&lt;P&gt;So I feel both the LPC-Link2 and MCU-Link are very well priced, and they support the NXP micro-controllers (LPC/Kinetis/RT). And the LPC-Link can be turned into a OEM Segger J-Link too (which I usually do).&lt;/P&gt;&lt;P&gt;Of course the other probes (PEMicro, Segger) have their own unique advantages, and I'm using them too.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Fri, 26 Mar 2021 05:28:39 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2021-03-26T05:28:39Z</dc:date>
    <item>
      <title>Realistically priced debugger/programmer for low volume users</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Realistically-priced-debugger-programmer-for-low-volume-users/m-p/1252494#M60005</link>
      <description>&lt;P&gt;Atmel, Microchip and STM all have ARM family mcu debuggers programmers available that are priced in the $100 or less price range [not starting at $599].&lt;/P&gt;&lt;P&gt;Even NXP has one for LPC ARM chips...for $25...&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;The LPC-Link 2 JTAG/SWD Debug probe brings exceptional value&lt;BR /&gt;to the LPCXpresso tool chain since its debugging functions can be&lt;BR /&gt;&lt;FONT face="andale mono,times" size="3" color="#0000FF"&gt;&lt;STRONG&gt;used with any other LPC evaluation board&lt;/STRONG&gt;&lt;/FONT&gt;. That means &lt;FONT size="3" color="#0000FF"&gt;&lt;STRONG&gt;engineers&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3" color="#0000FF"&gt;&lt;STRONG&gt;can use the same tools with other boards, including those used in&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3" color="#0000FF"&gt;&lt;STRONG&gt;final production&lt;/STRONG&gt;&lt;/FONT&gt;. &amp;lt;&amp;lt;&lt;/P&gt;&lt;P&gt;Now how about K series? Low cost eval boards...BUT the stinker is they CAN NOT be used on an external mcu chip even a prototype. It is at this point I moved to STM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 02:41:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Realistically-priced-debugger-programmer-for-low-volume-users/m-p/1252494#M60005</guid>
      <dc:creator>richardfritz</dc:creator>
      <dc:date>2021-03-26T02:41:41Z</dc:date>
    </item>
    <item>
      <title>Re: Realistically priced debugger/programmer for low volume users</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Realistically-priced-debugger-programmer-for-low-volume-users/m-p/1252602#M60010</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/128557"&gt;@richardfritz&lt;/a&gt; ,&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Even NXP has one for LPC ARM chips...for $25...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Not only LPC, but as well Kinetis and i.MX RT.&lt;/P&gt;&lt;P&gt;I use the LPC-Link2 (or embedded circuit of it on the boards) for all kind of the Kinetis devices (Kinetis-K, Kinetis-L for example) including the i.MX RT parts with the MCUXpresso IDE. You might be confused by the naming of the probe (agreed, probably for historical reasons), but it is *not* only for LPC, but as well for Kinetis and i.MX RT parts. Have a look at &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-link2:OM13054" target="_blank"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-link2:OM13054&lt;/A&gt; which lists the supported devices.&lt;/P&gt;&lt;P&gt;The LPC-Link2 is priced $20, but since some time there is the MCU-Link (notice the name) which is the successor of the LPC-Link2 and costs only $10 (see &lt;A href="https://www.nxp.com/design/development-boards/lpcxpresso-boards/mcu-link-debug-probe:MCU-LINK" target="_blank"&gt;https://www.nxp.com/design/development-boards/lpcxpresso-boards/mcu-link-debug-probe:MCU-LINK&lt;/A&gt; or my articles &lt;A href="https://mcuoneclipse.com/2020/11/29/new-mcu-link-debug-probe-from-nxp/" target="_blank"&gt;https://mcuoneclipse.com/2020/11/29/new-mcu-link-debug-probe-from-nxp/&lt;/A&gt; or &lt;A href="https://mcuoneclipse.com/tag/mcu-link/" target="_blank"&gt;https://mcuoneclipse.com/tag/mcu-link/&lt;/A&gt; ).&lt;/P&gt;&lt;P&gt;So I feel both the LPC-Link2 and MCU-Link are very well priced, and they support the NXP micro-controllers (LPC/Kinetis/RT). And the LPC-Link can be turned into a OEM Segger J-Link too (which I usually do).&lt;/P&gt;&lt;P&gt;Of course the other probes (PEMicro, Segger) have their own unique advantages, and I'm using them too.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 05:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Realistically-priced-debugger-programmer-for-low-volume-users/m-p/1252602#M60010</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-03-26T05:28:39Z</dc:date>
    </item>
  </channel>
</rss>