<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX examples for PK60FX512LQ120 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-examples-for-PK60FX512LQ120/m-p/145887#M6</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone successfully mated the libraries for the K60FX with MQX? &amp;nbsp;I have a twrK60N board which runs MQX demos just fine and I have proprietary HW that runs the Kinetis-sc bare metal demos just fine. When I try to bring the new MK60F102m libraries and MQX together I run into a host of problems some of which are simply new names for registers, but others are more challenging.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Mar 2012 12:05:05 GMT</pubDate>
    <dc:creator>MarkW_</dc:creator>
    <dc:date>2012-03-14T12:05:05Z</dc:date>
    <item>
      <title>MQX examples for PK60FX512LQ120</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-examples-for-PK60FX512LQ120/m-p/145887#M6</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone successfully mated the libraries for the K60FX with MQX? &amp;nbsp;I have a twrK60N board which runs MQX demos just fine and I have proprietary HW that runs the Kinetis-sc bare metal demos just fine. When I try to bring the new MK60F102m libraries and MQX together I run into a host of problems some of which are simply new names for registers, but others are more challenging.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Mar 2012 12:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-examples-for-PK60FX512LQ120/m-p/145887#M6</guid>
      <dc:creator>MarkW_</dc:creator>
      <dc:date>2012-03-14T12:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: MQX examples for PK60FX512LQ120</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-examples-for-PK60FX512LQ120/m-p/145888#M7</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think I have encountered a similar problem. I am trying to develop a BSP for our custom K60 board. I downloaded the MQX Board Support Package Porting Guide, Rev 0, 06/2011 and followed the directions for Chapter 3 CodeWarrior 10 BSP Creation. I used the bsp_twrk60n512_pe BSP project for my example to copy. I created the project and it built without error. The K60 Tower CPU board uses a PK50N512VMD100. Our board uses a PK60FX512VLQ12. I deleted the CPU from the project and used Processor Expert to add the MK60FX512VLQ12 processor to the project. I generated the ProcessorExpert code, cleaned and built the project. The build failed with 2,400 errors; all related to being various symbols and defines being redefined, or illegal name overloading. All of the errors were flagged in file IO_Map.h. I cannot track down any redefinition and text searches of the workspace do not yield any redefinitions. Is this a cockpit error on my part?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2012 22:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-examples-for-PK60FX512LQ120/m-p/145888#M7</guid>
      <dc:creator>nancyb</dc:creator>
      <dc:date>2012-04-20T22:58:12Z</dc:date>
    </item>
  </channel>
</rss>