<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMKE15Z256 Debug Vs Flash Programming</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1249807#M59952</link>
    <description>&lt;P&gt;I am thinking of using MKE15Z256 64pins for a new project. I also plan to use the LPC-Link2 card to record the flash and debug.&lt;/P&gt;&lt;P&gt;I read that I can use a 10-pin JTAG / SWD plug to connect the LPC-Link2 to the MKS15Z256, it will use SWDIO and SWCLK. But in the meantime I have the following doubt, with these two wires will I be able to debug or just record the flash?&lt;/P&gt;&lt;P&gt;I think the NXP documentation on the topic is very confusing. I was reading a document external to the NXP about Programming Internal Flash by SWD and in the description of the SWD standard is referred to 3 wires, SWDIO, SWCLK and SWO, the latter, Serial Wire Output is used for debugging. I looked for this pin on the MKE15Z256 but I didn't find it, I think that there is no.&lt;/P&gt;&lt;P&gt;Will I be able to debug only with SWDIO and SWCLK? Is there any clear documentation on this topic?&lt;/P&gt;&lt;P&gt;I was checking the FRDM-KE15Z development board and it in the openSDA block has a 10-pin JTAG / SWD connector but TDO and TDI are available and I was wondering if they are really needed for debugging.&amp;nbsp;On the other hand, the JTAG / SWD plug of the target uController only has SWDIO and SWCLCK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Mar 2021 16:46:07 GMT</pubDate>
    <dc:creator>Jmir</dc:creator>
    <dc:date>2021-03-22T16:46:07Z</dc:date>
    <item>
      <title>MKE15Z256 Debug Vs Flash Programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1249807#M59952</link>
      <description>&lt;P&gt;I am thinking of using MKE15Z256 64pins for a new project. I also plan to use the LPC-Link2 card to record the flash and debug.&lt;/P&gt;&lt;P&gt;I read that I can use a 10-pin JTAG / SWD plug to connect the LPC-Link2 to the MKS15Z256, it will use SWDIO and SWCLK. But in the meantime I have the following doubt, with these two wires will I be able to debug or just record the flash?&lt;/P&gt;&lt;P&gt;I think the NXP documentation on the topic is very confusing. I was reading a document external to the NXP about Programming Internal Flash by SWD and in the description of the SWD standard is referred to 3 wires, SWDIO, SWCLK and SWO, the latter, Serial Wire Output is used for debugging. I looked for this pin on the MKE15Z256 but I didn't find it, I think that there is no.&lt;/P&gt;&lt;P&gt;Will I be able to debug only with SWDIO and SWCLK? Is there any clear documentation on this topic?&lt;/P&gt;&lt;P&gt;I was checking the FRDM-KE15Z development board and it in the openSDA block has a 10-pin JTAG / SWD connector but TDO and TDI are available and I was wondering if they are really needed for debugging.&amp;nbsp;On the other hand, the JTAG / SWD plug of the target uController only has SWDIO and SWCLCK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 16:46:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1249807#M59952</guid>
      <dc:creator>Jmir</dc:creator>
      <dc:date>2021-03-22T16:46:07Z</dc:date>
    </item>
    <item>
      <title>Re: MKE15Z256 Debug Vs Flash Programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1249968#M59962</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This picture is from the arm debug interface specification.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140319iFADB8992D2014938/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.PNG" alt="1.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 01:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1249968#M59962</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-03-23T01:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: MKE15Z256 Debug Vs Flash Programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1250506#M59971</link>
      <description>&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;You can to share a link to the document that you refer?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 14:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1250506#M59971</guid>
      <dc:creator>Jmir</dc:creator>
      <dc:date>2021-03-23T14:19:26Z</dc:date>
    </item>
    <item>
      <title>Re: MKE15Z256 Debug Vs Flash Programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1250758#M59984</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please see the attachment&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 01:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE15Z256-Debug-Vs-Flash-Programming/m-p/1250758#M59984</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-03-24T01:41:33Z</dc:date>
    </item>
  </channel>
</rss>