<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Voltage on VBAt pin in K60 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241716#M5992</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you check TWR-K60D100M tower board, you could find below schematics about VBAT circuit, which provides battery power and board power selection with VBAT pin.&lt;/P&gt;&lt;P&gt;There is no need to set any register before using the VBAT pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="VBAT.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40757iB7C9898B4EA79E69/image-size/large?v=v2&amp;amp;px=999" role="button" title="VBAT.jpg" alt="VBAT.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;About RTC_WAKEUP open drain phenomenon, I need to check with Kinetis product engineer.&lt;/P&gt;&lt;P&gt;I will let you know when I could get any feedback.&lt;/P&gt;&lt;P&gt;Thank you for the patience.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 22 Sep 2013 01:24:06 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2013-09-22T01:24:06Z</dc:date>
    <item>
      <title>Voltage on VBAt pin in K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241715#M5991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use MK60DN512 MCU for my project. In my customized board I'm going to use the RTC and wakeup pin for power management purposes. I just noticed that there is a 3.3 V on VBAT pin which comes directly from CPU (no battery connected)! Based on datasheet this pin is supposed to be an isolated Input pin. So, I wonder if I should set up some registers before using this pin or something else going on here? I have 4 customized boards which all of them have the same issue (3 voltage on the VBAT). &lt;/P&gt;&lt;P&gt;Below you can see our schematic for this part. (Header 2 is battery which is not connected).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Sina&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="VBAT.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40379i71BAE3578C8F6E80/image-size/large?v=v2&amp;amp;px=999" role="button" title="VBAT.JPG" alt="VBAT.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Apparently, there is a relationship between VBAT and RTC wakeup pin. Based on the datasheet RTC wakeup pin is an open drain, active low output. so, we connect this pin to a 10K pullup resistor (as you can see below). If we increase this pull up to like 100k the VBAT pin voltage drops from 3V to 1.7V! So, I wonder if this wakeup pin is not a real open drain! Is there any internal pullup resistor on this pin? is there any leakage current from wakeup pin to the CPU? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="wakeup pin.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12826i1DED7B75895F1339/image-size/large?v=v2&amp;amp;px=999" role="button" title="wakeup pin.jpg" alt="wakeup pin.jpg" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2013 23:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241715#M5991</guid>
      <dc:creator>amleng</dc:creator>
      <dc:date>2013-09-19T23:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage on VBAt pin in K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241716#M5992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you check TWR-K60D100M tower board, you could find below schematics about VBAT circuit, which provides battery power and board power selection with VBAT pin.&lt;/P&gt;&lt;P&gt;There is no need to set any register before using the VBAT pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="VBAT.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40757iB7C9898B4EA79E69/image-size/large?v=v2&amp;amp;px=999" role="button" title="VBAT.jpg" alt="VBAT.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;About RTC_WAKEUP open drain phenomenon, I need to check with Kinetis product engineer.&lt;/P&gt;&lt;P&gt;I will let you know when I could get any feedback.&lt;/P&gt;&lt;P&gt;Thank you for the patience.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Sep 2013 01:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241716#M5992</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-09-22T01:24:06Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage on VBAt pin in K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241717#M5993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do a test with TWR-K60D100M RTC_WAKEUP pin, I use 100K ohm pull up resistor connects with RTC_WAKEUP pin, the voltage is 3.22V (VDD is 3.3V). &lt;/P&gt;&lt;P&gt;I also test to use 500K ohm pull up resistor connects with RTC_WAKEUP pin, the voltage is 2.87V (VDD is 3.3V).&lt;/P&gt;&lt;P&gt;If you could remove the RTC_WAKEUP pin peripheral circuit and &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; measure that pin related voltage.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Wish it helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2013 01:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241717#M5993</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-09-23T01:47:45Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage on VBAt pin in K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241718#M5994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui Ma, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually this is my point. If the wake up pin is an open drain pin it shouldn't be changed by external load. to me it's a bug in the silicon!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2013 20:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241718#M5994</guid>
      <dc:creator>amleng</dc:creator>
      <dc:date>2013-09-23T20:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage on VBAt pin in K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241719#M5995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Amleng&lt;/P&gt;&lt;P&gt;As you know, open-drain pin using as an input pin will cost very low current than normal IO. But open-drain has no drive ability, its input voltage level depends on external circuit. So I think the external load can effect wakeup pin input voltage. I suggest you have a check on your wake-up pin circuit. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2013 01:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Voltage-on-VBAt-pin-in-K60/m-p/241719#M5995</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-09-25T01:41:18Z</dc:date>
    </item>
  </channel>
</rss>