<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MK40DN512ZVLQ10 5n22d Mask</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1246645#M59909</link>
    <description>&lt;P&gt;Hello Sebastian thanks for responding.&lt;BR /&gt;I apologize for the delay, but I have been busy with other things and only now have I returned to work on this problem.&lt;BR /&gt;Well I didn't find anything in the errata that could be related to my problem.&lt;/P&gt;&lt;P&gt;I am using a universal P&amp;amp;E micro multilink to launch the file (BDM boot) on the target MCU.&lt;/P&gt;&lt;P&gt;After that I use the freescale universal bootloader software win_hc08sprg.exe.&lt;BR /&gt;I do these two processes in MCU targets MK40DN512ZVLQ10 with mask 4N30D and 5N22D and nothing points me to errors or problems in the process.&lt;BR /&gt;However, the MK40DN512ZVLQ10 4N30D target works normally and the MK40DN512ZVLQ10 5N22D simply does nothing.&lt;/P&gt;&lt;P&gt;Thank you very much and best regards&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 20:13:09 GMT</pubDate>
    <dc:creator>rbarbatana</dc:creator>
    <dc:date>2021-03-16T20:13:09Z</dc:date>
    <item>
      <title>MK40DN512ZVLQ10 5n22d Mask</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1196504#M59088</link>
      <description>&lt;P&gt;I'm having problems with the MK40DN512ZVLQ10 microcontroller, all my devices with this microcontroller with the 4n30d mask work normally.&lt;BR /&gt;However recently I received a batch of microcontrollers with the 5N22D mask.&lt;BR /&gt;I load the boot normally by JTAG and also the firmware by win_hc08sprg, but my devices just don't start, I read that there is an error regarding this 5n22d mask, but I can't see a relationship with the error that happens to me, can someone help me?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 14:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1196504#M59088</guid>
      <dc:creator>rbarbatana</dc:creator>
      <dc:date>2020-12-09T14:30:19Z</dc:date>
    </item>
    <item>
      <title>Re: MK40DN512ZVLQ10 5n22d Mask</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1199926#M59122</link>
      <description>&lt;P&gt;Hi Rafael, I hope you're doing well!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;According to the Kinetis Mask Set Errata 5N22D document &lt;A href="https://www.nxp.com/docs/en/errata/KINETIS_5N22D.pdf" target="_blank"&gt;here&lt;/A&gt;, the different erratum relating to JTAG and cJTAG are the following:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;e6804:&amp;nbsp;&amp;nbsp; CJTAG: Performing a mode change from Standard Protocol to AdvancedProtocol may reset the CJTAG&lt;/LI&gt;
&lt;LI&gt;e6990:&amp;nbsp;&amp;nbsp; CJTAG: possible incorrect TAP state machine advance during Check Packet&lt;/LI&gt;
&lt;LI&gt;e6573:&amp;nbsp;&amp;nbsp; JTAG: JTAG TDO function on the PTA2 disables the pull resistor&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There're workarounds to these errata in their respective sections on the errata document, however, this exact behavior hasn't been experienced before, could you please provide some more information about your issue?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sebastian.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 22:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1199926#M59122</guid>
      <dc:creator>Sebastian_Del_Rio</dc:creator>
      <dc:date>2020-12-15T22:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: MK40DN512ZVLQ10 5n22d Mask</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1246645#M59909</link>
      <description>&lt;P&gt;Hello Sebastian thanks for responding.&lt;BR /&gt;I apologize for the delay, but I have been busy with other things and only now have I returned to work on this problem.&lt;BR /&gt;Well I didn't find anything in the errata that could be related to my problem.&lt;/P&gt;&lt;P&gt;I am using a universal P&amp;amp;E micro multilink to launch the file (BDM boot) on the target MCU.&lt;/P&gt;&lt;P&gt;After that I use the freescale universal bootloader software win_hc08sprg.exe.&lt;BR /&gt;I do these two processes in MCU targets MK40DN512ZVLQ10 with mask 4N30D and 5N22D and nothing points me to errors or problems in the process.&lt;BR /&gt;However, the MK40DN512ZVLQ10 4N30D target works normally and the MK40DN512ZVLQ10 5N22D simply does nothing.&lt;/P&gt;&lt;P&gt;Thank you very much and best regards&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 20:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK40DN512ZVLQ10-5n22d-Mask/m-p/1246645#M59909</guid>
      <dc:creator>rbarbatana</dc:creator>
      <dc:date>2021-03-16T20:13:09Z</dc:date>
    </item>
  </channel>
</rss>