<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problems about Vector Table Remapping of KV11 Series： in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-about-Vector-Table-Remapping-of-KV11-Series/m-p/1242842#M59842</link>
    <description>&lt;DIV class="trans-left"&gt;&lt;DIV class="trans-input-wrap"&gt;&lt;DIV class="input-wrap"&gt;&lt;DIV class="textarea-wrap without-textarea-bg"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Recently, I have a project to implement IAP function on kv11, but I can't find the operation instructions for remapping the interrupt vector table. After checking the reference manual, I found that there is a register VTOR used to control the offset of&amp;nbsp; the interrupt vector table, but i couldn't find the operation about VTOR from the driver library. How can I remap the interrupt vector table?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;DIV class="trans-left"&gt;&lt;DIV class="trans-input-wrap"&gt;&lt;DIV class="input-wrap"&gt;&lt;DIV class="textarea-wrap without-textarea-bg"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="input-operate"&gt;&lt;DIV class="op-favor-container"&gt;&lt;SPAN&gt;It's better to show me the detailed sequence, thanks.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 10 Mar 2021 02:21:07 GMT</pubDate>
    <dc:creator>Saiwenliang</dc:creator>
    <dc:date>2021-03-10T02:21:07Z</dc:date>
    <item>
      <title>Problems about Vector Table Remapping of KV11 Series：</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-about-Vector-Table-Remapping-of-KV11-Series/m-p/1242842#M59842</link>
      <description>&lt;DIV class="trans-left"&gt;&lt;DIV class="trans-input-wrap"&gt;&lt;DIV class="input-wrap"&gt;&lt;DIV class="textarea-wrap without-textarea-bg"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Recently, I have a project to implement IAP function on kv11, but I can't find the operation instructions for remapping the interrupt vector table. After checking the reference manual, I found that there is a register VTOR used to control the offset of&amp;nbsp; the interrupt vector table, but i couldn't find the operation about VTOR from the driver library. How can I remap the interrupt vector table?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;DIV class="trans-left"&gt;&lt;DIV class="trans-input-wrap"&gt;&lt;DIV class="input-wrap"&gt;&lt;DIV class="textarea-wrap without-textarea-bg"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="input-operate"&gt;&lt;DIV class="op-favor-container"&gt;&lt;SPAN&gt;It's better to show me the detailed sequence, thanks.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 10 Mar 2021 02:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-about-Vector-Table-Remapping-of-KV11-Series/m-p/1242842#M59842</guid>
      <dc:creator>Saiwenliang</dc:creator>
      <dc:date>2021-03-10T02:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: Problems about Vector Table Remapping of KV11 Series：</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-about-Vector-Table-Remapping-of-KV11-Series/m-p/1242939#M59844</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You can refer this link.&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDMK64F-SD-Bootloader/ta-p/1099807" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDMK64F-SD-Bootloader/ta-p/1099807&lt;/A&gt;. Notice the figure 9.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 05:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problems-about-Vector-Table-Remapping-of-KV11-Series/m-p/1242939#M59844</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-03-10T05:22:28Z</dc:date>
    </item>
  </channel>
</rss>