<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK70 SPI Framesize</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-SPI-Framesize/m-p/1241175#M59807</link>
    <description>&lt;P&gt;mcu: K70FX512VMJ12&lt;/P&gt;&lt;P&gt;I'm trying to get a new LCD screen going but i need to send 9 bit spi packets (see image). On the K70, I tried to change the framesize to 9 but the LCD still does not communicate. I don't want to write a bit-bang SPI driver, so can the framesize be set to 9?&amp;nbsp; I send the data as a uint16, but im not sure if the SPI is sending the extra zeros.&amp;nbsp; I might need to hook up a scope.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LCDSPIST7_1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138917iDEC214C4AEA9A1DD/image-dimensions/477x214?v=v2" alt="LCDSPIST7_1.PNG" title="LCDSPIST7_1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;See code below. I want to make sure this is the proper way to send 9 bit packets.&lt;/P&gt;&lt;P&gt;In my initialize function I change the frame size to 9bits (along with other spi init):&lt;/P&gt;&lt;P&gt;// 9bit frame size&lt;BR /&gt;param = 9;&lt;BR /&gt;if (SPI_OK != ioctl(spiFileHandle, IO_IOCTL_SPI_SET_FRAMESIZE, &amp;amp;param))&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; printf ("Error: unable to set LCD SPI interface\n");&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Here is my spi write function:&lt;/P&gt;&lt;P&gt;static void SPI_Write(uint16_t i)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; int_32 result = 0;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; uint_16 retryCount = SPI_RETRY_COUNT;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; uint_32 param = 0;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; // Toggle CS1 Low&lt;BR /&gt;&amp;nbsp; &amp;nbsp; SetOutput(nSPI0_PCS1_OUTPUT, FALSE);&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; // Write Command/Data to SPI&lt;BR /&gt;&amp;nbsp; &amp;nbsp; retryCount = SPI_RETRY_COUNT;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; do&lt;BR /&gt;&amp;nbsp; &amp;nbsp; {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; result = fwrite((void *)&amp;amp;i, 2, 1, spiFileHandle);&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; retryCount--;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; }&lt;BR /&gt;&amp;nbsp; &amp;nbsp; while ((result &amp;lt; 1) &amp;amp;&amp;amp; (retryCount &amp;gt; 0));&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; // Toggle CS1 High&lt;BR /&gt;&amp;nbsp; &amp;nbsp; SetOutput(nSPI0_PCS1_OUTPUT, TRUE);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Mar 2021 18:33:24 GMT</pubDate>
    <dc:creator>MarkyNXP</dc:creator>
    <dc:date>2021-03-05T18:33:24Z</dc:date>
    <item>
      <title>K70 SPI Framesize</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-SPI-Framesize/m-p/1241175#M59807</link>
      <description>&lt;P&gt;mcu: K70FX512VMJ12&lt;/P&gt;&lt;P&gt;I'm trying to get a new LCD screen going but i need to send 9 bit spi packets (see image). On the K70, I tried to change the framesize to 9 but the LCD still does not communicate. I don't want to write a bit-bang SPI driver, so can the framesize be set to 9?&amp;nbsp; I send the data as a uint16, but im not sure if the SPI is sending the extra zeros.&amp;nbsp; I might need to hook up a scope.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LCDSPIST7_1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138917iDEC214C4AEA9A1DD/image-dimensions/477x214?v=v2" alt="LCDSPIST7_1.PNG" title="LCDSPIST7_1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;See code below. I want to make sure this is the proper way to send 9 bit packets.&lt;/P&gt;&lt;P&gt;In my initialize function I change the frame size to 9bits (along with other spi init):&lt;/P&gt;&lt;P&gt;// 9bit frame size&lt;BR /&gt;param = 9;&lt;BR /&gt;if (SPI_OK != ioctl(spiFileHandle, IO_IOCTL_SPI_SET_FRAMESIZE, &amp;amp;param))&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; printf ("Error: unable to set LCD SPI interface\n");&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Here is my spi write function:&lt;/P&gt;&lt;P&gt;static void SPI_Write(uint16_t i)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; int_32 result = 0;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; uint_16 retryCount = SPI_RETRY_COUNT;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; uint_32 param = 0;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; // Toggle CS1 Low&lt;BR /&gt;&amp;nbsp; &amp;nbsp; SetOutput(nSPI0_PCS1_OUTPUT, FALSE);&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; // Write Command/Data to SPI&lt;BR /&gt;&amp;nbsp; &amp;nbsp; retryCount = SPI_RETRY_COUNT;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; do&lt;BR /&gt;&amp;nbsp; &amp;nbsp; {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; result = fwrite((void *)&amp;amp;i, 2, 1, spiFileHandle);&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; retryCount--;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; }&lt;BR /&gt;&amp;nbsp; &amp;nbsp; while ((result &amp;lt; 1) &amp;amp;&amp;amp; (retryCount &amp;gt; 0));&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; // Toggle CS1 High&lt;BR /&gt;&amp;nbsp; &amp;nbsp; SetOutput(nSPI0_PCS1_OUTPUT, TRUE);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 18:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-SPI-Framesize/m-p/1241175#M59807</guid>
      <dc:creator>MarkyNXP</dc:creator>
      <dc:date>2021-03-05T18:33:24Z</dc:date>
    </item>
    <item>
      <title>Re: K70 SPI Framesize</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-SPI-Framesize/m-p/1242125#M59832</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;MarkyNXP,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;About the K70 SPI frame size,&amp;nbsp; it can support programmable serial frame size: 4 to 16 bits.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; You can configure it in this register:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1615259735738.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139059iFA35AD4CF7C69033/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1615259735738.png" alt="kerryzhou_0-1615259735738.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kerryzhou_0-1615259735738.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, please check your code, and debug the code, check the register, whether the above FMSZ is configured to 8? Then the real number of bits per frame should be 9.&lt;/P&gt;
&lt;P&gt;You also can test the SPI bus data which is sent out from K70, whether it is really 9 bits.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;If you still have questions about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 03:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-SPI-Framesize/m-p/1242125#M59832</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-03-09T03:19:14Z</dc:date>
    </item>
  </channel>
</rss>