<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMissing EHCI_STS_INT (USB interrupt USBINT, UI bit of USBHS_USBSTS) and failed enumeration</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1238614#M59766</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am implementing the USB stack on a Kinetis MK26FN2M0VMI18 using&amp;nbsp;Freescale BM USB Stack v5.0.&lt;/P&gt;&lt;P&gt;I am trying to implement an USB Virtual COM device.&lt;/P&gt;&lt;P&gt;Unlike the given examples in the BM USB Stack v5.0 sources, I have configured the stack to work with the EHCI controller by defining&amp;nbsp;HIGH_SPEED_DEVICE to 1.&lt;/P&gt;&lt;P&gt;When I attach the device to the PC USB port, I have&amp;nbsp;_usb_dci_usbhs_isr (ehci_dev_main.c) called and with&amp;nbsp;usb_hal_ehci_get_usb_status (USBHS_USBSTS register) there giving the following flags:&lt;/P&gt;&lt;P&gt;EHCI_STS_SUSPEND, EHCI_STS_RESET,&amp;nbsp;EHCI_STS_PORT_CHANGE, EHCI_STS_SUSPEND.&lt;/P&gt;&lt;P&gt;However, the&amp;nbsp;_usb_dci_usbhs_isr service routine is never called with&amp;nbsp;EHCI_STS_INT set (the UI bit of USBHS_USBSTS register), which would imply serving the GET_DESCRIPTOR request from the PC. Therefore, after some attempts, the PC gives up and finally it gives the message "Unrecognized USB device".&lt;/P&gt;&lt;P&gt;The interrupt is enabled: bit UE of&amp;nbsp;USBHS_USBINTR is set correctly.&lt;/P&gt;&lt;P&gt;Why don't I have&amp;nbsp;EHCI_STS_INT set?&lt;/P&gt;&lt;P&gt;Any hint?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Mar 2021 09:49:34 GMT</pubDate>
    <dc:creator>spiderman</dc:creator>
    <dc:date>2021-03-02T09:49:34Z</dc:date>
    <item>
      <title>Missing EHCI_STS_INT (USB interrupt USBINT, UI bit of USBHS_USBSTS) and failed enumeration</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1238614#M59766</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am implementing the USB stack on a Kinetis MK26FN2M0VMI18 using&amp;nbsp;Freescale BM USB Stack v5.0.&lt;/P&gt;&lt;P&gt;I am trying to implement an USB Virtual COM device.&lt;/P&gt;&lt;P&gt;Unlike the given examples in the BM USB Stack v5.0 sources, I have configured the stack to work with the EHCI controller by defining&amp;nbsp;HIGH_SPEED_DEVICE to 1.&lt;/P&gt;&lt;P&gt;When I attach the device to the PC USB port, I have&amp;nbsp;_usb_dci_usbhs_isr (ehci_dev_main.c) called and with&amp;nbsp;usb_hal_ehci_get_usb_status (USBHS_USBSTS register) there giving the following flags:&lt;/P&gt;&lt;P&gt;EHCI_STS_SUSPEND, EHCI_STS_RESET,&amp;nbsp;EHCI_STS_PORT_CHANGE, EHCI_STS_SUSPEND.&lt;/P&gt;&lt;P&gt;However, the&amp;nbsp;_usb_dci_usbhs_isr service routine is never called with&amp;nbsp;EHCI_STS_INT set (the UI bit of USBHS_USBSTS register), which would imply serving the GET_DESCRIPTOR request from the PC. Therefore, after some attempts, the PC gives up and finally it gives the message "Unrecognized USB device".&lt;/P&gt;&lt;P&gt;The interrupt is enabled: bit UE of&amp;nbsp;USBHS_USBINTR is set correctly.&lt;/P&gt;&lt;P&gt;Why don't I have&amp;nbsp;EHCI_STS_INT set?&lt;/P&gt;&lt;P&gt;Any hint?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Mar 2021 09:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1238614#M59766</guid>
      <dc:creator>spiderman</dc:creator>
      <dc:date>2021-03-02T09:49:34Z</dc:date>
    </item>
    <item>
      <title>Re: Missing EHCI_STS_INT (USB interrupt USBINT, UI bit of USBHS_USBSTS) and failed enumeration</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1239758#M59781</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43154"&gt;@spiderman&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This USB stack is a little old so the recommendation is to use the latest stack included in the &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_self"&gt;SDK&lt;/A&gt;, this package has multiple examples of how to use the different USB classes.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 23:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1239758#M59781</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-03-03T23:00:56Z</dc:date>
    </item>
    <item>
      <title>Re: Missing EHCI_STS_INT (USB interrupt USBINT, UI bit of USBHS_USBSTS) and failed enumeration</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1240427#M59788</link>
      <description>&lt;P&gt;OK thank you. We had also some hardware issue on the lines (removed capacitors, etc.). Seems to work for now at least with new hardware and latest stack.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 17:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-EHCI-STS-INT-USB-interrupt-USBINT-UI-bit-of-USBHS-USBSTS/m-p/1240427#M59788</guid>
      <dc:creator>spiderman</dc:creator>
      <dc:date>2021-03-04T17:45:33Z</dc:date>
    </item>
  </channel>
</rss>