<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Bootloader and buspal</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1234946#M59724</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;for my project I have two board with K64F microcontroller. One is master and have UART and one is slave and have only CAN. What I would like to do is have the possibility to program the master board directly via the blhost command or use the master borad to program the slave board via buspal.&lt;/P&gt;&lt;P&gt;To do this I should have bootloader, buspal and my application in flash memory for example booloader at 0x0000, buspal at 0xa000 and my application at 0x10000. My doubts are about how to do this.&lt;/P&gt;&lt;P&gt;In the bootloader code I saw there is a function&amp;nbsp;jump_to_application(applicationAddress, stackPointer) to jump to application that expect application address an stack pointer parameter that are calculated by&amp;nbsp;get_user_application_entry function. In my case for my application the address is 0x10000 but&amp;nbsp;where the stackpointer is obtained from?&lt;/P&gt;&lt;P&gt;Also I wanted to know if there is a description of the buspal protocol&amp;nbsp;to better understand which messages are sent for the various commands.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
    <pubDate>Tue, 23 Feb 2021 11:31:22 GMT</pubDate>
    <dc:creator>LArmstrong1985</dc:creator>
    <dc:date>2021-02-23T11:31:22Z</dc:date>
    <item>
      <title>Bootloader and buspal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1234946#M59724</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;for my project I have two board with K64F microcontroller. One is master and have UART and one is slave and have only CAN. What I would like to do is have the possibility to program the master board directly via the blhost command or use the master borad to program the slave board via buspal.&lt;/P&gt;&lt;P&gt;To do this I should have bootloader, buspal and my application in flash memory for example booloader at 0x0000, buspal at 0xa000 and my application at 0x10000. My doubts are about how to do this.&lt;/P&gt;&lt;P&gt;In the bootloader code I saw there is a function&amp;nbsp;jump_to_application(applicationAddress, stackPointer) to jump to application that expect application address an stack pointer parameter that are calculated by&amp;nbsp;get_user_application_entry function. In my case for my application the address is 0x10000 but&amp;nbsp;where the stackpointer is obtained from?&lt;/P&gt;&lt;P&gt;Also I wanted to know if there is a description of the buspal protocol&amp;nbsp;to better understand which messages are sent for the various commands.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 11:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1234946#M59724</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2021-02-23T11:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and buspal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1235122#M59729</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was able to do what I wanted.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, I have a doubt about the linker file of the two applications (.ld)&lt;/P&gt;&lt;P&gt;Currently the start address is different but they both have the same size of the text area (of the entire flash) and the same stack position.&lt;BR /&gt;Everything seems to work the same but is that correct?&lt;/P&gt;&lt;P&gt;Below is an excerpt of the two linker files:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;linker file app 1 (0xa000):&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;MEMORY&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;{&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;m_interrupts (RX) : ORIGIN = 0x0000a000, LENGTH = 0x00000400&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;m_flash_config (RX) : ORIGIN = 0x0000a400, LENGTH = 0x00000010&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;m_text (RX) : ORIGIN = 0x0000a410, LENGTH = 0x000FFBF0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00040000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;}&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="4"&gt;&lt;FONT face="courier new,courier"&gt;linker file app 2 (0x10000):&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7"&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;m_interrupts (RX) : ORIGIN = 0x00010000, LENGTH = 0x00000400&lt;BR /&gt;m_flash_config (RX) : ORIGIN = 0x00010400, LENGTH = 0x00000010&lt;BR /&gt;m_text (RX) : ORIGIN = 0x00010410, LENGTH = 0x000FFBF0&lt;BR /&gt;m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00040000&lt;BR /&gt;}&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="4"&gt;Thank you in advance!&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 17:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1235122#M59729</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2021-02-23T17:14:31Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and buspal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1236388#M59741</link>
      <description>&lt;P&gt;Hi fabiobenevento,&lt;/P&gt;
&lt;P&gt;It is fine. When jump to buspal, the bootloader's work is end. It's stack can be reused.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 07:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bootloader-and-buspal/m-p/1236388#M59741</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-02-25T07:06:51Z</dc:date>
    </item>
  </channel>
</rss>