<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFlash/CPU error on S32K1xx</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-CPU-error-on-S32K1xx/m-p/1227962#M59556</link>
    <description>&lt;P&gt;Hello Together,&lt;/P&gt;&lt;P&gt;i have some problems with a S32K142&lt;/P&gt;&lt;P&gt;I was able to debug and flash the device for quite some time.&lt;/P&gt;&lt;P&gt;Now, after i had some connection problems, i can still connect to the Debug-Interface (via Segger Jlink) but it tells me that the either CPU cannot be halted or that the device is in permanent reset .&lt;BR /&gt;After connecting the reset-pin to GND and another access via Jlink, I tried to unlock the device (which was successful).&lt;/P&gt;&lt;P&gt;After this, i can - sometimes - access the memory, but it keeps changing the content which is shown.&lt;/P&gt;&lt;P&gt;erase/flash/etc. is not possible&lt;/P&gt;&lt;P&gt;I tried SWD and JTAG, i also changed the speed.&lt;/P&gt;&lt;P&gt;As far as i can see from the datasheet, the device cannot start the internal RC Oscillator to provide a clock to the CPU and the memory.&lt;/P&gt;&lt;P&gt;To give some more hint: because i had an error in the design, i provided a signal on a pin before i had a power connected. I resolved the problem, so this was not happening any more at the time the above error occured.&lt;/P&gt;&lt;P&gt;Is it possible that i ruined the port or the oscillator unit with the "supply via ESD Diode"?&lt;/P&gt;&lt;P&gt;It doesn't seem that i had a latch-up because the ports still worked fine (and the connection via SWD/JTAG is still possible).&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Roland&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Feb 2021 12:42:02 GMT</pubDate>
    <dc:creator>sero</dc:creator>
    <dc:date>2021-02-08T12:42:02Z</dc:date>
    <item>
      <title>Flash/CPU error on S32K1xx</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-CPU-error-on-S32K1xx/m-p/1227962#M59556</link>
      <description>&lt;P&gt;Hello Together,&lt;/P&gt;&lt;P&gt;i have some problems with a S32K142&lt;/P&gt;&lt;P&gt;I was able to debug and flash the device for quite some time.&lt;/P&gt;&lt;P&gt;Now, after i had some connection problems, i can still connect to the Debug-Interface (via Segger Jlink) but it tells me that the either CPU cannot be halted or that the device is in permanent reset .&lt;BR /&gt;After connecting the reset-pin to GND and another access via Jlink, I tried to unlock the device (which was successful).&lt;/P&gt;&lt;P&gt;After this, i can - sometimes - access the memory, but it keeps changing the content which is shown.&lt;/P&gt;&lt;P&gt;erase/flash/etc. is not possible&lt;/P&gt;&lt;P&gt;I tried SWD and JTAG, i also changed the speed.&lt;/P&gt;&lt;P&gt;As far as i can see from the datasheet, the device cannot start the internal RC Oscillator to provide a clock to the CPU and the memory.&lt;/P&gt;&lt;P&gt;To give some more hint: because i had an error in the design, i provided a signal on a pin before i had a power connected. I resolved the problem, so this was not happening any more at the time the above error occured.&lt;/P&gt;&lt;P&gt;Is it possible that i ruined the port or the oscillator unit with the "supply via ESD Diode"?&lt;/P&gt;&lt;P&gt;It doesn't seem that i had a latch-up because the ports still worked fine (and the connection via SWD/JTAG is still possible).&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Roland&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 12:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-CPU-error-on-S32K1xx/m-p/1227962#M59556</guid>
      <dc:creator>sero</dc:creator>
      <dc:date>2021-02-08T12:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: Flash/CPU error on S32K1xx</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-CPU-error-on-S32K1xx/m-p/1228071#M59564</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/62"&gt;@admin&lt;/a&gt;: can you delete this please? i moved it to S32K subforum&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 15:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-CPU-error-on-S32K1xx/m-p/1228071#M59564</guid>
      <dc:creator>sero</dc:creator>
      <dc:date>2021-02-08T15:29:17Z</dc:date>
    </item>
  </channel>
</rss>