<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Interfacing external I2C device with K66F dev kit in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-external-I2C-device-with-K66F-dev-kit/m-p/1227132#M59538</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to interface an external sensor with the firmware running on Free RTOS.&lt;/P&gt;&lt;P&gt;There are examples for I2C ports from 2 different boards or 2 different&amp;nbsp; I2C ports from the same board.&lt;/P&gt;&lt;P&gt;from my understanding, The idea is to use drivers and wrapper from "fsl_i2c_freertos" and that inturn uses "fsl_i2c"&lt;/P&gt;&lt;P&gt;But how to find the properties of external slave device for "I2C_Type" ?&lt;/P&gt;&lt;P&gt;There are only the slave address and registers to read the data from the external sensor.&lt;/P&gt;&lt;P&gt;Any links to example or info could be helpful.&lt;/P&gt;&lt;P&gt;Also, When I try to run a simple example program , the single board version communication between 2 I2C ports from the same board (i.e. "frdm66f_freertos_i2c") I get "kStatus_I2C_Addr_Nak"&lt;/P&gt;&lt;P&gt;What could be the error?&lt;/P&gt;&lt;P&gt;Thanks in Advance!&lt;/P&gt;</description>
    <pubDate>Sat, 06 Feb 2021 14:56:27 GMT</pubDate>
    <dc:creator>viveknath_thulasi</dc:creator>
    <dc:date>2021-02-06T14:56:27Z</dc:date>
    <item>
      <title>Interfacing external I2C device with K66F dev kit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-external-I2C-device-with-K66F-dev-kit/m-p/1227132#M59538</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to interface an external sensor with the firmware running on Free RTOS.&lt;/P&gt;&lt;P&gt;There are examples for I2C ports from 2 different boards or 2 different&amp;nbsp; I2C ports from the same board.&lt;/P&gt;&lt;P&gt;from my understanding, The idea is to use drivers and wrapper from "fsl_i2c_freertos" and that inturn uses "fsl_i2c"&lt;/P&gt;&lt;P&gt;But how to find the properties of external slave device for "I2C_Type" ?&lt;/P&gt;&lt;P&gt;There are only the slave address and registers to read the data from the external sensor.&lt;/P&gt;&lt;P&gt;Any links to example or info could be helpful.&lt;/P&gt;&lt;P&gt;Also, When I try to run a simple example program , the single board version communication between 2 I2C ports from the same board (i.e. "frdm66f_freertos_i2c") I get "kStatus_I2C_Addr_Nak"&lt;/P&gt;&lt;P&gt;What could be the error?&lt;/P&gt;&lt;P&gt;Thanks in Advance!&lt;/P&gt;</description>
      <pubDate>Sat, 06 Feb 2021 14:56:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-external-I2C-device-with-K66F-dev-kit/m-p/1227132#M59538</guid>
      <dc:creator>viveknath_thulasi</dc:creator>
      <dc:date>2021-02-06T14:56:27Z</dc:date>
    </item>
  </channel>
</rss>