<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KE18F Single Bit ECC Interrupt/Reporting</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-Single-Bit-ECC-Interrupt-Reporting/m-p/1225776#M59521</link>
    <description>&lt;P&gt;The KE18F has a mechanism in the FTFE module to generate an interrupt for double bit errors using the&amp;nbsp;FTFE_FERSTAT[DFDIF].&lt;/P&gt;&lt;P&gt;Is there something similar for reporting single bit errors?&lt;/P&gt;&lt;P&gt;Would doing a margin read fill the role of determining single bit errors?&lt;/P&gt;</description>
    <pubDate>Wed, 03 Feb 2021 19:36:19 GMT</pubDate>
    <dc:creator>sean_dvorscak</dc:creator>
    <dc:date>2021-02-03T19:36:19Z</dc:date>
    <item>
      <title>KE18F Single Bit ECC Interrupt/Reporting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-Single-Bit-ECC-Interrupt-Reporting/m-p/1225776#M59521</link>
      <description>&lt;P&gt;The KE18F has a mechanism in the FTFE module to generate an interrupt for double bit errors using the&amp;nbsp;FTFE_FERSTAT[DFDIF].&lt;/P&gt;&lt;P&gt;Is there something similar for reporting single bit errors?&lt;/P&gt;&lt;P&gt;Would doing a margin read fill the role of determining single bit errors?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 19:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-Single-Bit-ECC-Interrupt-Reporting/m-p/1225776#M59521</guid>
      <dc:creator>sean_dvorscak</dc:creator>
      <dc:date>2021-02-03T19:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: KE18F Single Bit ECC Interrupt/Reporting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-Single-Bit-ECC-Interrupt-Reporting/m-p/1226198#M59527</link>
      <description>&lt;P&gt;Hi sean,&lt;/P&gt;
&lt;P&gt;No, there isn't flag which can report single bit error.&lt;/P&gt;
&lt;P&gt;You can use margin read to check flash array. But I doubt if it can pick out single error bit. Since it is on the margin level, the error bit&amp;nbsp; may jump out randomly. Margin check has a certain pattern, for example, write all zero -&amp;gt; all one -&amp;gt; 0x5555aaaa -&amp;gt; 0xaaaa5555. And then change the margin level and do again.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 08:05:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE18F-Single-Bit-ECC-Interrupt-Reporting/m-p/1226198#M59527</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-02-04T08:05:03Z</dc:date>
    </item>
  </channel>
</rss>