<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: What's the minimum circuit requirement for KL/K mcu programming?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241285#M5950</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniele,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the programmer work OK with the on-board KL25 chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also make sure you have programmed a dummy program to the on-board chip before using the external programmer. See at the bottom of this page:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/freedom_setup.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/freedom_setup.html"&gt;USBDM: Setting Up the FRDM-KL25Z&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The waveform you are seeing is to be expected from a blank chip.&amp;nbsp; The target device will be resetting itself due to either a watchdog timer expiration or due to executing an illegal instruction.&amp;nbsp; I've never bothered determining which.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should not interfere with the programming.&amp;nbsp; I have confirmed this with a few different chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the stand-alone programmer detect the device at all?&lt;/P&gt;&lt;P&gt;Also selecting mass erase will usually be more reliable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Apr 2014 10:20:40 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2014-04-17T10:20:40Z</dc:date>
    <item>
      <title>What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241268#M5933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying my best to use FRDM on board OpenSDA debugger to program hex/srec/bin code into off-board KL25Z/K20 boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the following errors:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Keil + CMSIS-DAP firmware, SWD/JTAG communication error&lt;/LI&gt;&lt;LI&gt;IAR + PEmicro OpenSDA firmware, a setup window popup to show no target MCU found.&lt;/LI&gt;&lt;LI&gt;Coocox + CoLinkEX + CoFlash, &lt;STRONG&gt;"Flash not blank !!! -&amp;gt; Can NOT Stop MCU !!!"&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SWD should be the simplest way to program a cortex micro.&amp;nbsp; (VCC/GND, DIO/CLK/RST) I have double checked the connections. They are good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I have changed a TXC 8MHz crystal in these boards. I want to know if the crystal can influence the SWD programming? Is it possible to program a bare KL25Z chip (only MCU mounted on board, not crystal, only SWD connections are available, and power source comes from SWD as well) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far I don't think cystal issue is the root cause of programming failure, because KL25Z can run from IRC. FSL can not enforce customer to add crystal for programming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is surprise to me when I failed in programming KL25Z with FRDM+CMSIS-DAP. &lt;A href="http://blog.sina.com.cn/s/blog_4680937f0101qnms.html"&gt;This CMSIS-DAP programming configuration &lt;/A&gt;is even working well for other MCU. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 08:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241268#M5933</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-02-18T08:52:59Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241269#M5934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The most basic circuitry you need is the power rail [VDD and VSS] connections, the decoupling capacitors for VDD, and pull-up resistors in the RST and SWD_DIO pins. By default the MCU starts up in FEI mode, thus; there is no need to use an external CLK source such as a XTAL. Also be very mindful of the cable connecting between your programming probe and the mcu; it must not be longer than 4 inches.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41486iC52CF8697A060370/image-size/large?v=v2&amp;amp;px=999" title="SWD interface.bmp" alt="SWD interface.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 21:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241269#M5934</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2014-02-18T21:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241270#M5935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is a PDF showing a &lt;STRONG&gt;very&lt;/STRONG&gt; minimal KL05 chip design I used for testing the USBDM programmer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that it is important to have the power supply capacitors otherwise the device programs erratically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 01:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241270#M5935</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-02-19T01:27:26Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241271#M5936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo, &lt;/P&gt;&lt;P&gt;why you do not put a pull-up resister in swdio pin ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 03:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241271#M5936</guid>
      <dc:creator>rqbh</dc:creator>
      <dc:date>2014-02-19T03:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241272#M5937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pedro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have pull up resistors on SWD_DIO as well as RESET. For my understanding, The pull-up is useful in JTAG debugger JTAG_TMS. The pull up resistor maybe drawn somewhere in reset circuit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, I will try to check them all over again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 08:03:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241272#M5937</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-02-19T08:03:28Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241273#M5938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks. I will check the decouping caps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 08:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241273#M5938</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-02-19T08:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241274#M5939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tested again for programming my custom KL25Z boardwith OpenSDA of FRDM-KL25Z. Still fails on SWD communication error. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Debug Proble&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am not good at hardware debugging so I list my checklist here.&lt;/P&gt;&lt;P&gt;Cross checking with Cortex-M0+ mini board with LPC812 (NXP), success.&lt;/P&gt;&lt;P&gt;Cross checking with Cortex-M0+ mini board with LPC811 (NXP), success.&lt;/P&gt;&lt;P&gt;Cross checking with Crotex-M0 mini board with LPC1114F (NXP), success.&lt;/P&gt;&lt;P&gt;OpenSDA with KL25Z, fails (communication error).&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Conclusion: board issues caused by KL25Z, OpenSDA works well.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Power supply&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Check power supply, 3.3V regulated. (both from OpenSDA 3.3V pin headers as well as LDO from KL25Z board)&lt;/P&gt;&lt;P&gt;Check ground, done.&lt;/P&gt;&lt;P&gt;Decoupling caps, soldered. done.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Conclusion: Very good power supply with common ground.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Cables&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Wire connection (RST/DIO/CLK), good, less than 10 Ohm (using IDC cable as well as other shorter wires as cross checking)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Power up measurement&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;VCC:3V, RST:3V, DIO:3V, CLK:3V (NXP board)&lt;/P&gt;&lt;P&gt;VCC:3V, RST:1.5V, DIO:0V, CLK:0V (KL25Z)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Reset Circuit?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;It seems RST is not stable or keep MCU in reset state. I checked my schematics &amp;amp; PCB layout.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42852i2A1339F3D76BDF52/image-size/large?v=v2&amp;amp;px=999" title="KL25Z_RST_SCH.png" alt="KL25Z_RST_SCH.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Shematics (EAGLE)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reset of SWD connects to MCU, and push button with 10K weak pull-up and 1uF to ground. (Although 1uF cap to GND looks big, but it is same as FRDM.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, I also tested (not fully tests) on a bare PCB with only SWD sockets and MCU on board. The reset connection from SWD to MCU is short enough, and 10K pull-up and 1uF to GND are empty. The reset should be fully under control of OpenSDA. Why this happens again? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my last attempt programming with CoLinkEx, which use buffer IC to drive reset as well. It will reports "CAN NOT STOP MCU". Is there anything I should take care of reset?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42853i710AD430835212DE/image-size/large?v=v2&amp;amp;px=999" title="KL25Z_RST.png" alt="KL25Z_RST.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PCB (EAGLE)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PCB routing looks bad, it almost route three corners of the whole board. You can identify the right side SWD socket, the most right down corner is reset, then you can find the reset net links to reset pad, the other branch goes up, goes left most, before goes down to push button and 10K resistor and 1uF cap. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far I can only find this "suspicious". &lt;STRONG&gt;Any comments are highly welcome.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since it is my first FSL hardware platform, I will like to ask help from FSL experts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 03:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241274#M5939</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-02-26T03:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241275#M5940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The minimal circuit I posted above has been used OK with a FRDM-KL25 used as programmer board using USBDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you try this arrangement with USBDM as a sanity check i.e. a known working arrangement identical to your hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL chips can be hard to reset "fresh" from the factory as they may be in a reset loop.&amp;nbsp; Still, most programmers should be able to cope with this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a side note.&amp;nbsp; You appear to be using pins 7 &amp;amp; 9 of the SWD connector for a serial port.&amp;nbsp; I suggest you not use pin 7 as it reserved for a key pin so (in theory) there will be some programming cables that will not be able to be physically connected to your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 04:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241275#M5940</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-02-26T04:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241276#M5941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, I will try USBDM to find out if it can work on that board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is really surprised to me to know that KL chips are hard to reset. Does FSL mention that in some documents? I did spent hours to find how to reset it properly. When it is powered up, the reset is kept on 1.5V (half VCC) with 10K pull-up resistor. I tried to replace pull-up with 1K/470R/220R/100R, I can only get the reset on 2V, but that really bugs me. And it doesn't work at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my understanding, reset should be Schimitt trigger, which is totally works as input with high impedance. A 10K pull-up should be able to pull reset pin to VCC. I have no idea why it only pulls it on 1.5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PIN7/PIN9 are designed for RX/TX, but I will drop this since I have already realize that is risky.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 08:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241276#M5941</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-02-26T08:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241277#M5942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A Kinetis chip with an invalid program may suffer from several kinds of program errors:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Failure to reset or disable the watchdog timer&lt;/LI&gt;&lt;LI&gt;Bus lockup on illegal program execution (illegal instruction or illegal address etc)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;These will lead to the chip resetting itself.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This can be observed by&amp;nbsp; examining the reset pin with an oscilloscope.&amp;nbsp; It will be seen to be pulsing low by itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This can lead to problems since a reset may occur part way through the connection sequence.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2014 05:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241277#M5942</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-02-27T05:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241278#M5943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This morning I have tried CoLinkEX to access all four boards at hand. Only one can be connected, programmed and verified in Coocox's CoFlash. I verified the level of reset, it is 3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am still trying to make a device description file for KL25Z used in Keil/Coocox driver to debug the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I connect these four boards to USBDM (Kinetis) in ARM programmer, none can be connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Interface&lt;/STRONG&gt; tab: USBDM-OPENSDA-A0001 detected&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Target&lt;/STRONG&gt; tab: Device detect =&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Connection with target has failed.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Please cycle power to the target (measured vcc to gnd, 3V)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Retry connection?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Failed to detect chips&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Reason: BDM has no connection to target.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Advanced&lt;/STRONG&gt; tab:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I try to load OpenSDAMassEraseKinetis.sx to mass erase target KL25Z?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Lab 1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used OpenSDAMassEraseKinetis to earse external KL25Z by removing J11/J4 jumpers. And I followed the instructions from OpenSDAMassEraseKinetis.txt. By power up cycle, the LED flash rate keep 50% on/off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's going wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Lab 2&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used SEGGER J-Flash ARM, it can be detected via SWD, however I am using a clone version of J-Link. So ... Keil refused to work with a clone version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Lab 3&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am using J-LINK lite for OpenSDA, the device can be connected via SWD in J-Flash. But reading back memory is failed .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;RAM check failed @ address 0x1FFFF000.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Write: 0x03020100 07060504&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Read: 0x00000000 00000000&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(0 bytes of RAM have been checked successfully)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Failed to check blank target.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe SWD_DIO has bad connection ? But if can be connected, DIO should be good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems I should visit FSL.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 00:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241278#M5943</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-02-28T00:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241279#M5944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now I found there is 125KHz signal comes from reset pin, check thread on &lt;A _jive_internal="true" href="https://community.nxp.com/message/384630#384630"&gt;https://community.freescale.com/message/384630#384630&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42935i7BE84C0C64CB427A/image-size/large?v=v2&amp;amp;px=999" title="KL25Z_RST_Saleae_Screenshot.PNG.png" alt="KL25Z_RST_Saleae_Screenshot.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now I found it, but I have no idea how to solve it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Mar 2014 00:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241279#M5944</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-03-02T00:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241280#M5945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well. I would like to update for this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As pgo said, 125KHz output is normal in new sample. I visited FSL Shanghai this morning and met Mr. Peng Wang in the office. Up to now, we can draw some conclusions and some &lt;SPAN style="color: #000000; font-family: Arial; font-size: 12px;"&gt;speculates so far.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Fact 1:&lt;/STRONG&gt; None of these boards can be connected to most of the debugger. (&lt;STRONG&gt;Speculate: They may have been damaged during POR&lt;/STRONG&gt;, due to improper PCB layout, like long and narrow GND and long trace for reset which may introduces too much noise )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Fact 2:&lt;/STRONG&gt; By adding more decoupling capacitor and replacing with a new KL25Z, it talks to JLINK (clone) in command mode (The new KL25Z can be detected with following info with a script from Mr. Wang:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="plain" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13951323743463336" jivemacro_uid="_13951323743463336"&gt;
&lt;P&gt;Reset delay: 0 ms&lt;/P&gt;
&lt;P&gt;Reset type RESETPIN: Resets core &amp;amp; peripherals using RESET pin.&lt;/P&gt;
&lt;P&gt;Info: Found SWD-DP with ID 0x0BC11477&lt;/P&gt;
&lt;P&gt;Info: FPUnit: 2 code (BP) slots and 0 literal slots&lt;/P&gt;
&lt;P&gt;Info: Found Cortex-M0 r0p0, Little endian.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;R0 = 00000023, R1 = 1FFFF410, R2 = 00000000, R3 = 00000000&lt;/P&gt;
&lt;P&gt;R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000&lt;/P&gt;
&lt;P&gt;R8 = 002001B0, R9 = 01489800, R10= 886084A0, R11= 04420B2C&lt;/P&gt;
&lt;P&gt;R12= 840982DF, R13= FFFFFFFC, MSP= FFFFFFFC, PSP= 33012A20&lt;/P&gt;
&lt;P&gt;R14(LR) = 00000A1D, R15(PC) = FFFFFFFE&lt;/P&gt;
&lt;P&gt;XPSR 81000000, APSR 80000000, EPSR 01000000, IPSR 00000000&lt;/P&gt;
&lt;P&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;/P&gt;

&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Fact 3:&lt;/STRONG&gt; However, it still can not talk to other debugger, including OpenSDA/CMSIS-DAP/CoLinkEx in SWD mode. As a cross checking, these debugger can program on board KL25Z of FRDM-KL25Z.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Fact 4: &lt;/STRONG&gt;Although JLINK is the only one which can talk with KL25Z, but it refused to work because it is a clone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We don't have enough time to arrange an inspection over the circuit with oscilloscope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From viewpoint of schematics, it is working. But I have to revise the PCB with proper GND, shorter SWD connections.&lt;/P&gt;&lt;P&gt;However, I still have no idea how to debug it, or even download the code. Does JLINK commander support code programming?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 08:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241280#M5945</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-03-18T08:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241281#M5946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I added a series resistor on SWD_CLK, then most of debuggers can talk to KL25Z.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MultiLink (Passed)&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;PEmicro for OpenSDA/FRDM (&lt;STRONG&gt;Failed, because its driver is overwritten by Multilink?&lt;/STRONG&gt;)&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;JLINK for OpenSDA/FRDM (Passed)&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;CMSIS-DAP for OpenSDA/FRDM &lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;(Passed)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;USBDM for OpenSDA/FRDM &lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;(Passed)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;CooCox CoLinkEX &lt;SPAN style="color: #333333; font-family: 'normal tahoma', Verdana, Arial; font-size: 12px;"&gt;(&lt;STRONG&gt;Failed, check cable&lt;/STRONG&gt;)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;Some FAE told me that is impedance matching. I don't know, 1MHz SWD clk requires impedance matching circuit? I used to think only 100MHz + requires impedance matching.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;Anyway, we can close this issue now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;Well, let me thank people who have helped me out of that. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pgo"&gt;pgo&lt;/A&gt;, thanks for point me to right direction, from silicon to my board. I hope it doesn't bug you too much.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/speer"&gt;speer&lt;/A&gt; &amp;amp; Gary Guo, thanks for assign FAE to help me.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;Mr. Wang Peng, thanks for your profesional services and precious time to replace damaged samples on board and offer me more samples to test. and tell me the hardware design principles.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;FAE ConstYu, thanks your comments on Chinese FSL community, for adding resistor on CLK.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;FuMing, my friend, thanks for allowing me to use your debugger.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;Yours sincerely&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;Allan K Liu&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;A class="jive-link-external-small" href="http://allankliu.blogspot.com/"&gt;http://allankliu.blogspot.com/&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;A class="jive-link-external-small" href="http://blog.sina.com.cn/allankliu/"&gt;http://blog.sina.com.cn/allankliu/&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #333333; font-size: 12px; font-family: 'normal tahoma', Verdana, Arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 01:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241281#M5946</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-03-19T01:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241282#M5947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, same problem on my board. I have a voltage of 1.5V on the reset pin with usbdm programmer. Tomorrow i will read the pin with an oscilloscope and try your solution. I have tried three different kl25 and all with the same problem. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Apr 2014 20:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241282#M5947</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2014-04-16T20:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241283#M5948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniele,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What USBDM programmer are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 07:38:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241283#M5948</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-04-17T07:38:16Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241284#M5949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using USBDM like here &lt;A href="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;Using the Freedom Board as SWD Programmer | MCU on Eclipse&lt;/A&gt;. I have tried different solution but the problem still. &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44080iD51B8D3B52C3D738/image-size/large?v=v2&amp;amp;px=999" title="F0001TEK.JPG.jpg" alt="F0001TEK.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is the signal that i read on the reset pin with this circuit&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43872iFF840A276FA0213E/image-size/large?v=v2&amp;amp;px=999" title="Immagine.JPG.jpg" alt="Immagine.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;if i add this resistence of 470R&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43919i884E785AAA26E1B7/image-size/large?v=v2&amp;amp;px=999" title="Immagine1.JPG.jpg" alt="Immagine1.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;i see this signal on the reset pin&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44028i49E773199920AC89/image-size/large?v=v2&amp;amp;px=999" title="F0003TEK.JPG.jpg" alt="F0003TEK.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the problem is that the signal is only 1.5V, then i can't program the micro. I don't understand why the kl25 continue to reset ....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 08:23:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241284#M5949</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2014-04-17T08:23:48Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241285#M5950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniele,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the programmer work OK with the on-board KL25 chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also make sure you have programmed a dummy program to the on-board chip before using the external programmer. See at the bottom of this page:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/freedom_setup.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/freedom_setup.html"&gt;USBDM: Setting Up the FRDM-KL25Z&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The waveform you are seeing is to be expected from a blank chip.&amp;nbsp; The target device will be resetting itself due to either a watchdog timer expiration or due to executing an illegal instruction.&amp;nbsp; I've never bothered determining which.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should not interfere with the programming.&amp;nbsp; I have confirmed this with a few different chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the stand-alone programmer detect the device at all?&lt;/P&gt;&lt;P&gt;Also selecting mass erase will usually be more reliable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 10:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241285#M5950</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-04-17T10:20:40Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241286#M5951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a frdm kl05 instead kl25, the programmer didn't have problem. I have two same boards, with one i didn't have problem but with this yes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 11:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241286#M5951</guid>
      <dc:creator>danielecortella</dc:creator>
      <dc:date>2014-04-17T11:28:15Z</dc:date>
    </item>
    <item>
      <title>Re: What's the minimum circuit requirement for KL/K mcu programming?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241287#M5952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How big is this series resistor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 14:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-s-the-minimum-circuit-requirement-for-KL-K-mcu-programming/m-p/241287#M5952</guid>
      <dc:creator>gokhanozcan</dc:creator>
      <dc:date>2014-09-23T14:51:37Z</dc:date>
    </item>
  </channel>
</rss>