<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cannot program with CMSIS-DAP and MCUXpresso in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-program-with-CMSIS-DAP-and-MCUXpresso/m-p/1224171#M59481</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've a strange problem with GUI FlashTool in MCUXpresso 11.2.1.&lt;/P&gt;&lt;P&gt;If I try to program my board with DapLink (CMSIS-DAP) when I click to Run... it do nothing&lt;/P&gt;&lt;P&gt;and&amp;nbsp;I'm not getting any errors. All works well instead when I use it in debug.&lt;/P&gt;&lt;P&gt;The problem is also present in other PCs with the coupled MCUXpresso 11.2 and Windows 10 20H2 while on another PC with MCUXpresso 11.1.0 and Windows 10 1909 all works fine.&lt;/P&gt;&lt;P&gt;I tried to downgrade MCUXpresso and Windows 10 in this PC but I was unable to resolve.&lt;/P&gt;&lt;P&gt;Does anyone else have the same problem?&amp;nbsp;Are you aware of compatibility problems with some versions of Windows or Mcuxpresso?&lt;/P&gt;&lt;P&gt;Thank you id advance&lt;/P&gt;</description>
    <pubDate>Mon, 01 Feb 2021 16:18:23 GMT</pubDate>
    <dc:creator>LArmstrong1985</dc:creator>
    <dc:date>2021-02-01T16:18:23Z</dc:date>
    <item>
      <title>Cannot program with CMSIS-DAP and MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-program-with-CMSIS-DAP-and-MCUXpresso/m-p/1224171#M59481</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've a strange problem with GUI FlashTool in MCUXpresso 11.2.1.&lt;/P&gt;&lt;P&gt;If I try to program my board with DapLink (CMSIS-DAP) when I click to Run... it do nothing&lt;/P&gt;&lt;P&gt;and&amp;nbsp;I'm not getting any errors. All works well instead when I use it in debug.&lt;/P&gt;&lt;P&gt;The problem is also present in other PCs with the coupled MCUXpresso 11.2 and Windows 10 20H2 while on another PC with MCUXpresso 11.1.0 and Windows 10 1909 all works fine.&lt;/P&gt;&lt;P&gt;I tried to downgrade MCUXpresso and Windows 10 in this PC but I was unable to resolve.&lt;/P&gt;&lt;P&gt;Does anyone else have the same problem?&amp;nbsp;Are you aware of compatibility problems with some versions of Windows or Mcuxpresso?&lt;/P&gt;&lt;P&gt;Thank you id advance&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 16:18:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-program-with-CMSIS-DAP-and-MCUXpresso/m-p/1224171#M59481</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2021-02-01T16:18:23Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot program with CMSIS-DAP and MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-program-with-CMSIS-DAP-and-MCUXpresso/m-p/1225305#M59506</link>
      <description>&lt;P&gt;Hi fabiobenevento,&lt;/P&gt;
&lt;P&gt;Can you use CMSIS-DAP to debug? If it can't debug too, maybe you can try to reinstall the driver.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;MCUXpresso IDE has updated to v11.3. If v11.2 can't work, you can update it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 07:17:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-program-with-CMSIS-DAP-and-MCUXpresso/m-p/1225305#M59506</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-02-03T07:17:06Z</dc:date>
    </item>
  </channel>
</rss>