<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 REST API on K64 with lwIP</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/REST-API-on-K64-with-lwIP/m-p/1224138#M59479</link>
    <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am using lwIP over K64 and I would add REST API to my project.&lt;/P&gt;&lt;P&gt;I try to understand how to do that, and the only way that I have found is to use CGI. The problem is the reply: I can reply only with a static file present in the SDCARD (the return of the following function is the address of the file.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;typedef const char *(*tCGIHandler)(int iIndex, int iNumParams, char *pcParam[],char *pcValue[]);&lt;/LI-CODE&gt;&lt;P&gt;Does someone return a JSON build at runtime?&lt;/P&gt;&lt;P&gt;Does someone parse a GET REST request build with / and not with &amp;amp;? How?&amp;nbsp;&lt;/P&gt;&lt;P&gt;api/test/1/3 indeed of api/test.cgi?arg=1&amp;amp;subarg=3&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
    <pubDate>Mon, 01 Feb 2021 14:44:16 GMT</pubDate>
    <dc:creator>MarcoGiammarini</dc:creator>
    <dc:date>2021-02-01T14:44:16Z</dc:date>
    <item>
      <title>REST API on K64 with lwIP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/REST-API-on-K64-with-lwIP/m-p/1224138#M59479</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am using lwIP over K64 and I would add REST API to my project.&lt;/P&gt;&lt;P&gt;I try to understand how to do that, and the only way that I have found is to use CGI. The problem is the reply: I can reply only with a static file present in the SDCARD (the return of the following function is the address of the file.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;typedef const char *(*tCGIHandler)(int iIndex, int iNumParams, char *pcParam[],char *pcValue[]);&lt;/LI-CODE&gt;&lt;P&gt;Does someone return a JSON build at runtime?&lt;/P&gt;&lt;P&gt;Does someone parse a GET REST request build with / and not with &amp;amp;? How?&amp;nbsp;&lt;/P&gt;&lt;P&gt;api/test/1/3 indeed of api/test.cgi?arg=1&amp;amp;subarg=3&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 14:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/REST-API-on-K64-with-lwIP/m-p/1224138#M59479</guid>
      <dc:creator>MarcoGiammarini</dc:creator>
      <dc:date>2021-02-01T14:44:16Z</dc:date>
    </item>
    <item>
      <title>Re: REST API on K64 with lwIP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/REST-API-on-K64-with-lwIP/m-p/1257618#M60103</link>
      <description>&lt;P&gt;Hi Marco:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would suggest you get help from lwip users forum for this question.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regard&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 03:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/REST-API-on-K64-with-lwIP/m-p/1257618#M60103</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-04-07T03:04:58Z</dc:date>
    </item>
  </channel>
</rss>