<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: SRM motor control with hall sensor</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRM-motor-control-with-hall-sensor/m-p/1211584#M59337</link>
    <description>&lt;P&gt;Hi, kaarthi,&lt;/P&gt;
&lt;P&gt;I think it is reasonable that phase current is high when you connect the load. Can you adjust the peak current threshold so that the current fault does not happen.&lt;/P&gt;
&lt;P&gt;Pls go to the link and download DRM100.pdf for the phase current waveform&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSCSHSSR-Sensorless-High-Speed-SR-Motor-Drive-for-Vacuum/ta-p/1115181" target="_blank"&gt;https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSCSHSSR-Sensorless-High-Speed-SR-Motor-Drive-for-Vacuum/ta-p/1115181&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jan 2021 08:04:53 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-01-14T08:04:53Z</dc:date>
    <item>
      <title>SRM motor control with hall sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRM-motor-control-with-hall-sensor/m-p/1210355#M59314</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using&lt;SPAN&gt;&amp;nbsp;MKV30F128 micro controller&amp;nbsp;&lt;/SPAN&gt;for controlling 3 phase SRM motor with hall sensor feedback for position measurement. I am able to rotate the motor in no load. In load the over current fault occurs even with low load. In no load also, the 3 phase currents are not equal. Anyone having experience with SRM motor control, kindly help me to solve this problem.&lt;/P&gt;&lt;P&gt;Note: feedback - magnet disc is attached with shaft and hall sensor is placed against it.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 11:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRM-motor-control-with-hall-sensor/m-p/1210355#M59314</guid>
      <dc:creator>Kaarthi</dc:creator>
      <dc:date>2021-01-12T11:36:44Z</dc:date>
    </item>
    <item>
      <title>Re: SRM motor control with hall sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRM-motor-control-with-hall-sensor/m-p/1211584#M59337</link>
      <description>&lt;P&gt;Hi, kaarthi,&lt;/P&gt;
&lt;P&gt;I think it is reasonable that phase current is high when you connect the load. Can you adjust the peak current threshold so that the current fault does not happen.&lt;/P&gt;
&lt;P&gt;Pls go to the link and download DRM100.pdf for the phase current waveform&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSCSHSSR-Sensorless-High-Speed-SR-Motor-Drive-for-Vacuum/ta-p/1115181" target="_blank"&gt;https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSCSHSSR-Sensorless-High-Speed-SR-Motor-Drive-for-Vacuum/ta-p/1115181&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 08:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRM-motor-control-with-hall-sensor/m-p/1211584#M59337</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-14T08:04:53Z</dc:date>
    </item>
  </channel>
</rss>