<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why are there ADC clock frequency minimum operating conditions? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-are-there-ADC-clock-frequency-minimum-operating-conditions/m-p/1205025#M59201</link>
    <description>&lt;P&gt;On the K10 datasheet (specifically the&amp;nbsp;MK10DX128VLK7) the 16-bit minimum clock frequency is different then the &amp;lt;= 13 bit clock frequency:&lt;/P&gt;&lt;P&gt;fADCK ADC conversion clock frequency ≤ 13-bit mode: 1.0 — 18.0 MHz&lt;BR /&gt;fADCK ADC conversion clock frequency 16-bit mode: 2.0 — 12.0 MHz&lt;BR /&gt;&lt;BR /&gt;Why is that? Why do are there minimum limits to the ADC frequency? And what happens if a clock frequency is used that is below this frequency?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I noticed this warning in Processor Expert when I was using a 1 MHz ADC frequency in 16-bit mode, but the clock configuration was a valid configuration other than this warning, and from what I can tell, it seemed to work fine. I need to know if this is critical to ADC functionality.&lt;/P&gt;</description>
    <pubDate>Tue, 29 Dec 2020 21:53:46 GMT</pubDate>
    <dc:creator>danebouchie</dc:creator>
    <dc:date>2020-12-29T21:53:46Z</dc:date>
    <item>
      <title>Why are there ADC clock frequency minimum operating conditions?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-are-there-ADC-clock-frequency-minimum-operating-conditions/m-p/1205025#M59201</link>
      <description>&lt;P&gt;On the K10 datasheet (specifically the&amp;nbsp;MK10DX128VLK7) the 16-bit minimum clock frequency is different then the &amp;lt;= 13 bit clock frequency:&lt;/P&gt;&lt;P&gt;fADCK ADC conversion clock frequency ≤ 13-bit mode: 1.0 — 18.0 MHz&lt;BR /&gt;fADCK ADC conversion clock frequency 16-bit mode: 2.0 — 12.0 MHz&lt;BR /&gt;&lt;BR /&gt;Why is that? Why do are there minimum limits to the ADC frequency? And what happens if a clock frequency is used that is below this frequency?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I noticed this warning in Processor Expert when I was using a 1 MHz ADC frequency in 16-bit mode, but the clock configuration was a valid configuration other than this warning, and from what I can tell, it seemed to work fine. I need to know if this is critical to ADC functionality.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 21:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-are-there-ADC-clock-frequency-minimum-operating-conditions/m-p/1205025#M59201</guid>
      <dc:creator>danebouchie</dc:creator>
      <dc:date>2020-12-29T21:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: Why are there ADC clock frequency minimum operating conditions?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-are-there-ADC-clock-frequency-minimum-operating-conditions/m-p/1205319#M59207</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/140074"&gt;@danebouchie&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The ADC module works with a minimum and maximum sample rate and this is to ensure the proper functionality of the module. Any value outside the specification, the proper behavior of the module is not guaranteed.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 21:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-are-there-ADC-clock-frequency-minimum-operating-conditions/m-p/1205319#M59207</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-12-30T21:56:28Z</dc:date>
    </item>
  </channel>
</rss>