<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Communication between FRDM-K66F and FPGA</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203247#M59164</link>
    <description>&lt;P&gt;Hello weijfh,&lt;/P&gt;&lt;P&gt;No, you can not transfer Data from two USB-Devices. You need a host in between. You could use for example a raspberry pie or a PC. Connect the two USB-Interfaces to it and run some code which bridges the two serial interfaces.&lt;/P&gt;&lt;P&gt;Alternatively, you can grab the RX and TX signals from the KC705 Board before the Silicon Labs USB to UART bridge and connect it directly to the K64 on TTL level.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
    <pubDate>Tue, 22 Dec 2020 22:27:16 GMT</pubDate>
    <dc:creator>Masmiseim</dc:creator>
    <dc:date>2020-12-22T22:27:16Z</dc:date>
    <item>
      <title>Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202022#M59146</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I trying to transfer data from microcontroller(FRDM-K66F) to FPGA(kc705) by uart. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I successfully transmitted data from FRDM-K66F to pc by uart and successfully received data from pc to KC705 by uart. However, I failed to transfer data from FRDM-K66FF to KC705.(Both FRDM-K66F and KC705 are 9600 baud rate, 8-bit data, 1 stop bit)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can anybody give some advice?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Wei-Chieh&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Dec 2020 15:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202022#M59146</guid>
      <dc:creator>weijfh</dc:creator>
      <dc:date>2020-12-20T15:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202023#M59147</link>
      <description>&lt;P&gt;Have you crossed Rx and Tx between K66 and KC705?&lt;/P&gt;</description>
      <pubDate>Sun, 20 Dec 2020 16:06:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202023#M59147</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2020-12-20T16:06:58Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202469#M59150</link>
      <description>&lt;P&gt;Hi Masmiseim,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Thank you for your reply.I have tried to swap Tx and Rx by exchanging the white line(D1) and brown line(D0). However, I still failed to receive data from K66.&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MCU_FPGA_UART.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133181i76ECE5938609D6B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="MCU_FPGA_UART.jpg" alt="MCU_FPGA_UART.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MCU_FPGA_UART.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 11:18:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202469#M59150</guid>
      <dc:creator>weijfh</dc:creator>
      <dc:date>2020-12-21T11:18:37Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202599#M59153</link>
      <description>&lt;P&gt;This is a long chain of adapters. There could be a lot of possible fault location.&lt;/P&gt;&lt;P&gt;I guess you have connected KC705 directly to the PC via a mini-b cable which is working as you said?&lt;/P&gt;&lt;P&gt;Have you used the same adapters as shown in the picture to connect the K64 to the PC? Do you used the same USB-to-TTL-Adapter without the Type-A-to-mini-b Adapter?&lt;/P&gt;&lt;P&gt;If this is the case, the Type-A-to-mini-b is only new Adapter in the chain of adapters? Are you Shure that this adapter is working?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 17:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1202599#M59153</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2020-12-21T17:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203029#M59157</link>
      <description>&lt;P&gt;Hello &lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181616" target="_blank"&gt;weijfh&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;one more thing I noticed. The &lt;/SPAN&gt;KC705 Board is a USB-Device with a virtual Serial-Port, correct? The USB-to-TTL adapter is also a USB-Device, connecting both together is not working. You need at least one USB-Master or OTG device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 10:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203029#M59157</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2020-12-22T10:24:36Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203089#M59158</link>
      <description>&lt;P&gt;Hi Masmiseim,&lt;/P&gt;&lt;P&gt;Thank you for quick reply.&lt;BR /&gt;1.) I tested the adapter by connecting it with USB-to-USB adapter to PC, and it works well.&lt;BR /&gt;2.) Yes, the KC705 is a USB-Device with a virtual Serial-Port. Does it mean that I can't transfer&lt;BR /&gt;data from K66F to KC705?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Wei-Chieh&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 13:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203089#M59158</guid>
      <dc:creator>weijfh</dc:creator>
      <dc:date>2020-12-22T13:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203247#M59164</link>
      <description>&lt;P&gt;Hello weijfh,&lt;/P&gt;&lt;P&gt;No, you can not transfer Data from two USB-Devices. You need a host in between. You could use for example a raspberry pie or a PC. Connect the two USB-Interfaces to it and run some code which bridges the two serial interfaces.&lt;/P&gt;&lt;P&gt;Alternatively, you can grab the RX and TX signals from the KC705 Board before the Silicon Labs USB to UART bridge and connect it directly to the K64 on TTL level.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 22:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203247#M59164</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2020-12-22T22:27:16Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between FRDM-K66F and FPGA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203318#M59167</link>
      <description>&lt;P&gt;Hi Masmiseim,&lt;/P&gt;&lt;P&gt;Thank you so much!&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Wei-Chieh&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 01:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Communication-between-FRDM-K66F-and-FPGA/m-p/1203318#M59167</guid>
      <dc:creator>weijfh</dc:creator>
      <dc:date>2020-12-23T01:53:54Z</dc:date>
    </item>
  </channel>
</rss>