<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックGenerate a 1MHz timer with low power timer driver</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-a-1MHz-timer-with-low-power-timer-driver/m-p/1202021#M59145</link>
    <description>&lt;P&gt;I have a KL03 board and I can generate a timer using the 1kHz LPO. However, I wanted to know if I can generate a 1MHz timer using a different clock as I am trying to interface with an HC-SR04 Ultrasound sensor.&lt;/P&gt;</description>
    <pubDate>Sun, 20 Dec 2020 15:19:52 GMT</pubDate>
    <dc:creator>Fayojimi</dc:creator>
    <dc:date>2020-12-20T15:19:52Z</dc:date>
    <item>
      <title>Generate a 1MHz timer with low power timer driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-a-1MHz-timer-with-low-power-timer-driver/m-p/1202021#M59145</link>
      <description>&lt;P&gt;I have a KL03 board and I can generate a timer using the 1kHz LPO. However, I wanted to know if I can generate a 1MHz timer using a different clock as I am trying to interface with an HC-SR04 Ultrasound sensor.&lt;/P&gt;</description>
      <pubDate>Sun, 20 Dec 2020 15:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-a-1MHz-timer-with-low-power-timer-driver/m-p/1202021#M59145</guid>
      <dc:creator>Fayojimi</dc:creator>
      <dc:date>2020-12-20T15:19:52Z</dc:date>
    </item>
    <item>
      <title>Re: Generate a 1MHz timer with low power timer driver</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-a-1MHz-timer-with-low-power-timer-driver/m-p/1202113#M59148</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;LPTMR&amp;nbsp; has four clock source.&amp;nbsp;MCGIRCLK,&amp;nbsp; LPO, ERCLK32K, OSCERCLK.&lt;/P&gt;
&lt;P&gt;You can use&amp;nbsp;MCGIRCLK to generate 1 Mhz.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 02:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-a-1MHz-timer-with-low-power-timer-driver/m-p/1202113#M59148</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-12-21T02:00:57Z</dc:date>
    </item>
  </channel>
</rss>