<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Mesh Network with BLE</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mesh-Network-with-BLE/m-p/1196244#M59082</link>
    <description>&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MKW-38 evaluation board for my project. It needs my evaluation board to be connected as slave to a master device via Bluetooth and also at the same time it needs to scan for nearby Bluetooth devices.&lt;/P&gt;&lt;P&gt;Does MKW-38 supports this and if yes, then please send me a link to documentation or an example code that I can refer for further development.&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Vipul&lt;/P&gt;</description>
    <pubDate>Wed, 09 Dec 2020 09:38:07 GMT</pubDate>
    <dc:creator>notanivipul</dc:creator>
    <dc:date>2020-12-09T09:38:07Z</dc:date>
    <item>
      <title>Mesh Network with BLE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mesh-Network-with-BLE/m-p/1196244#M59082</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MKW-38 evaluation board for my project. It needs my evaluation board to be connected as slave to a master device via Bluetooth and also at the same time it needs to scan for nearby Bluetooth devices.&lt;/P&gt;&lt;P&gt;Does MKW-38 supports this and if yes, then please send me a link to documentation or an example code that I can refer for further development.&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Vipul&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 09:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mesh-Network-with-BLE/m-p/1196244#M59082</guid>
      <dc:creator>notanivipul</dc:creator>
      <dc:date>2020-12-09T09:38:07Z</dc:date>
    </item>
    <item>
      <title>Re: Mesh Network with BLE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mesh-Network-with-BLE/m-p/1197100#M59095</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The example&amp;nbsp;w_uart meet your demand. For detailed information, you can refer attachment ,chapter 5.18. It has two roles in one device.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 05:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mesh-Network-with-BLE/m-p/1197100#M59095</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-12-10T05:30:49Z</dc:date>
    </item>
  </channel>
</rss>