<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LwIP and USB device in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1195229#M59064</link>
    <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I found two similar project, one of them you mantioned and the second: USB tethering host (RNDIS protocol) implementation for kinetis. So I started to developed my project based on them.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Dec 2020 07:08:02 GMT</pubDate>
    <dc:creator>Markon</dc:creator>
    <dc:date>2020-12-08T07:08:02Z</dc:date>
    <item>
      <title>LwIP and USB device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1194463#M59039</link>
      <description>&lt;P&gt;I'm working on project base on K66 processor. I have the latest SDK built with USB and LwIP stack. I need to use LwIP with USB device to connect to PC. I find file:&amp;nbsp;usb_ethernetif_freertos.c but it is for using USB host with LwIP.&lt;/P&gt;&lt;P&gt;Is there any similar file, which connect LwIP with USB device?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 06:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1194463#M59039</guid>
      <dc:creator>Markon</dc:creator>
      <dc:date>2020-12-07T06:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: LwIP and USB device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1195160#M59060</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The similar demo maybe the virtual NIC,&amp;nbsp; it is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a network adapter. Users can access the network by properly configuring this network adapter.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_0-1607406661611.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132061iE3DC9901381070ED/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielchen_0-1607406661611.png" alt="danielchen_0-1607406661611.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielchen_0-1607406661611.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 05:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1195160#M59060</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-12-08T05:51:52Z</dc:date>
    </item>
    <item>
      <title>Re: LwIP and USB device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1195229#M59064</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I found two similar project, one of them you mantioned and the second: USB tethering host (RNDIS protocol) implementation for kinetis. So I started to developed my project based on them.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 07:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/m-p/1195229#M59064</guid>
      <dc:creator>Markon</dc:creator>
      <dc:date>2020-12-08T07:08:02Z</dc:date>
    </item>
  </channel>
</rss>