<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMCU-LINK max UART baudrate</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194191#M59033</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What is the MCU-LINK maximum UART baudrate (VCOM header J7) with reliable UART transfer from free running (released from SWD) target device to PC?&lt;/P&gt;&lt;P&gt;BTW, I don't get it why is so hard today to put some product data in few-pages good old pdf.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
    <pubDate>Sat, 05 Dec 2020 16:49:49 GMT</pubDate>
    <dc:creator>jh0</dc:creator>
    <dc:date>2020-12-05T16:49:49Z</dc:date>
    <item>
      <title>MCU-LINK max UART baudrate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194191#M59033</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What is the MCU-LINK maximum UART baudrate (VCOM header J7) with reliable UART transfer from free running (released from SWD) target device to PC?&lt;/P&gt;&lt;P&gt;BTW, I don't get it why is so hard today to put some product data in few-pages good old pdf.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
      <pubDate>Sat, 05 Dec 2020 16:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194191#M59033</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2020-12-05T16:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-LINK max UART baudrate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194211#M59034</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/95980"&gt;@jh0&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm able to use it with 115200, see&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2020/11/29/new-mcu-link-debug-probe-from-nxp/" target="_blank"&gt;https://mcuoneclipse.com/2020/11/29/new-mcu-link-debug-probe-from-nxp/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Sat, 05 Dec 2020 19:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194211#M59034</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2020-12-05T19:07:23Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-LINK max UART baudrate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194238#M59035</link>
      <description>&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;Thank you for all this things published on mcuoneclipse.&lt;/P&gt;&lt;P&gt;115200 is supported by all flashing / debugging master devices and this is not what I am looking for. I need highest possible baudrate in MBits for log from free running target device. I am using my 4 MBps CDC / UART bridge for this, but want to have it (flasher / bridge) in one device.&lt;/P&gt;</description>
      <pubDate>Sun, 06 Dec 2020 07:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1194238#M59035</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2020-12-06T07:50:36Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-LINK max UART baudrate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1349985#M61624</link>
      <description>&lt;P&gt;Just to close this older topic...&lt;/P&gt;&lt;P&gt;There is noted inside &lt;STRONG&gt;UM11673 MCU-Link Pro User Manual &lt;/STRONG&gt;at the end of &lt;STRONG&gt;4.3 VCOM (USB to Target UART bridge)&lt;/STRONG&gt; ...&lt;/P&gt;&lt;P&gt;"Baud rates of up to 5.33Mbps are supported."&lt;/P&gt;&lt;P&gt;I checked this with MCU-Link (non Pro) updated to latest firmware v2.245, and UART bridge is working fine on 4 Mbps.&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;It is also working fine on 4.8 and 5.33 Mbps.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Oct 2021 05:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-LINK-max-UART-baudrate/m-p/1349985#M61624</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2021-10-18T05:42:27Z</dc:date>
    </item>
  </channel>
</rss>