<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kinetis ke04 NMI pin in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-ke04-NMI-pin/m-p/1185722#M59002</link>
    <description>&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;The NMI pin is open because it is unused. If the default settings after power-on reset are used, will NMI be applied without pulling up externally?&lt;BR /&gt;Also, if NMI is not used, are there any registers that should be set in relation to NMI?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Nov 2020 04:12:57 GMT</pubDate>
    <dc:creator>jun1</dc:creator>
    <dc:date>2020-11-19T04:12:57Z</dc:date>
    <item>
      <title>kinetis ke04 NMI pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-ke04-NMI-pin/m-p/1185722#M59002</link>
      <description>&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;The NMI pin is open because it is unused. If the default settings after power-on reset are used, will NMI be applied without pulling up externally?&lt;BR /&gt;Also, if NMI is not used, are there any registers that should be set in relation to NMI?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 04:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-ke04-NMI-pin/m-p/1185722#M59002</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2020-11-19T04:12:57Z</dc:date>
    </item>
  </channel>
</rss>