<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K10 Watchdog Timeout Setting in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/1188425#M58920</link>
    <description>&lt;P&gt;So, to have 4s delay:&amp;nbsp;&lt;BR /&gt;WDOG_TOVALH=0x0&lt;/P&gt;&lt;P&gt;WDOG_TOVALL=0x0FA0&lt;/P&gt;&lt;P&gt;Am I correct ?&lt;/P&gt;&lt;P&gt;Thank you very much in advance for the reply.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 20:31:28 GMT</pubDate>
    <dc:creator>Oleksii</dc:creator>
    <dc:date>2020-11-24T20:31:28Z</dc:date>
    <item>
      <title>K10 Watchdog Timeout Setting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/612019#M36227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to configure the watchdog timer on my K10. More precisely I can't find a formula to fill-in WDOG_TOVALH and WDOG_TOVALL from my timeout value expressed in seconds (or ms). I'm using LPO clock and WDOG_PRES is set to 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 13:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/612019#M36227</guid>
      <dc:creator>maxpag</dc:creator>
      <dc:date>2016-12-14T13:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: K10 Watchdog Timeout Setting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/612020#M36228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The Watchdog Time-out Value Register defined in terms of cycles of the watchdog clock. WDOG_TOVALL defines the upper 16 bits of the 32-bit time-out value for the watchdog timer, and WDOG_TOVALL defines the lower 16 bits of the 32-bit time-out value for the watchdog timer.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10297i1F7023A189D0C66E/image-size/large?v=v2&amp;amp;px=999" title="WDOG_TOVAL.png" alt="WDOG_TOVAL.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since you are using 1kHz LPO clock and WDOG_PRES is set to 0, one watchdog clock cycle is 1ms.&lt;/P&gt;&lt;P&gt;Your timeout value expressed in ms will equal to the 32-bit time-out value for the watchdog timer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 06:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/612020#M36228</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-12-15T06:19:29Z</dc:date>
    </item>
    <item>
      <title>Re: K10 Watchdog Timeout Setting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/1188425#M58920</link>
      <description>&lt;P&gt;So, to have 4s delay:&amp;nbsp;&lt;BR /&gt;WDOG_TOVALH=0x0&lt;/P&gt;&lt;P&gt;WDOG_TOVALL=0x0FA0&lt;/P&gt;&lt;P&gt;Am I correct ?&lt;/P&gt;&lt;P&gt;Thank you very much in advance for the reply.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 20:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Watchdog-Timeout-Setting/m-p/1188425#M58920</guid>
      <dc:creator>Oleksii</dc:creator>
      <dc:date>2020-11-24T20:31:28Z</dc:date>
    </item>
  </channel>
</rss>