<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 .</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unreadable-title/m-p/1186993#M58891</link>
    <description>&lt;P&gt;Hey guys,I need some help!&lt;/P&gt;&lt;P&gt;I'm working on a . and i'm trying to display a message on a 16X2 LCD using..&lt;/P&gt;&lt;P&gt;I'm still not able to find a useful tutorial or code.&lt;/P&gt;&lt;P&gt;Could someone help me with the code for it or me give some guidance on how to program the code?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 20:44:53 GMT</pubDate>
    <dc:creator>Raul_CN</dc:creator>
    <dc:date>2020-11-24T20:44:53Z</dc:date>
    <item>
      <title>.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unreadable-title/m-p/1186993#M58891</link>
      <description>&lt;P&gt;Hey guys,I need some help!&lt;/P&gt;&lt;P&gt;I'm working on a . and i'm trying to display a message on a 16X2 LCD using..&lt;/P&gt;&lt;P&gt;I'm still not able to find a useful tutorial or code.&lt;/P&gt;&lt;P&gt;Could someone help me with the code for it or me give some guidance on how to program the code?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 20:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/unreadable-title/m-p/1186993#M58891</guid>
      <dc:creator>Raul_CN</dc:creator>
      <dc:date>2020-11-24T20:44:53Z</dc:date>
    </item>
    <item>
      <title>Re: Having trouble interfacing an I2C LCD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/unreadable-title/m-p/1186997#M58892</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178658"&gt;@Raul_CN&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've got some experience in this area.&lt;/P&gt;&lt;P&gt;To be honest, you're probably not going to find any references that are going to be exact - you're going to have to create your own code.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fortunately, you have two things in your favour.&amp;nbsp; 1. the SDK code is pretty good for doing standard I2C operations and can be expanded to include DMA (although probably not required if it's a 16x2 character LCD) and 2. I2C, because of the definite Ack from the receiver you will know when you're communicating (even with out an oscilloscope, although I highly recommend having one to look at the lines).&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the device you're trying to connect to and what datasheet/resources (for the display as well as its controller) are available?&amp;nbsp; Often there will be Arduino libraries that can help show you the way.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;</description>
      <pubDate>Sun, 22 Nov 2020 01:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/unreadable-title/m-p/1186997#M58892</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2020-11-22T01:54:53Z</dc:date>
    </item>
  </channel>
</rss>