<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K22 USB OTG with Silicon Labs CP2104</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-USB-OTG-with-Silicon-Labs-CP2104/m-p/1176164#M58694</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am working on a project that requires, me to connect a Silicon Labs CP2104 (USB to UART converter) to a K22 USB Host / OTG port. Currently, not using any OS on the K22 and the code is all bare metal in C (IAR EWB).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wanted to check if this is possible and if any similar efforts have been made by others, that I can use as a reference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA.&lt;/P&gt;</description>
    <pubDate>Sat, 31 Oct 2020 07:26:56 GMT</pubDate>
    <dc:creator>ET_Dev</dc:creator>
    <dc:date>2020-10-31T07:26:56Z</dc:date>
    <item>
      <title>K22 USB OTG with Silicon Labs CP2104</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-USB-OTG-with-Silicon-Labs-CP2104/m-p/1176164#M58694</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am working on a project that requires, me to connect a Silicon Labs CP2104 (USB to UART converter) to a K22 USB Host / OTG port. Currently, not using any OS on the K22 and the code is all bare metal in C (IAR EWB).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wanted to check if this is possible and if any similar efforts have been made by others, that I can use as a reference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA.&lt;/P&gt;</description>
      <pubDate>Sat, 31 Oct 2020 07:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-USB-OTG-with-Silicon-Labs-CP2104/m-p/1176164#M58694</guid>
      <dc:creator>ET_Dev</dc:creator>
      <dc:date>2020-10-31T07:26:56Z</dc:date>
    </item>
  </channel>
</rss>