<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-KE02Z40M and CodeWarrior in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176092#M58688</link>
    <description>&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I am new to using NXP (Freescale) 32-bit micros. Do I need CodeWarrior (and which version) to write and flash code into the FRDM-KE02Z40M board?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 30 Oct 2020 20:45:24 GMT</pubDate>
    <dc:creator>Circuit_Man</dc:creator>
    <dc:date>2020-10-30T20:45:24Z</dc:date>
    <item>
      <title>FRDM-KE02Z40M and CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176092#M58688</link>
      <description>&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I am new to using NXP (Freescale) 32-bit micros. Do I need CodeWarrior (and which version) to write and flash code into the FRDM-KE02Z40M board?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 20:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176092#M58688</guid>
      <dc:creator>Circuit_Man</dc:creator>
      <dc:date>2020-10-30T20:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE02Z40M and CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176097#M58689</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Your processor/board can be used with various IDEs but CodeWarrior is a rather old one that is no longer officially supported, which means that it is probably best to use a more modern one.&lt;BR /&gt;You can try the open source uTasker project that supports your processor/board with almost any IDE rather than being restricted to the ones that NXP presently supports:&lt;BR /&gt;&lt;A href="https://github.com/uTasker/uTasker-Kinetis" target="_blank"&gt;https://github.com/uTasker/uTasker-Kinetis&lt;/A&gt;&lt;BR /&gt;Compliers/IDEs: &lt;A href="https://www.utasker.com/kinetis/compilers.html" target="_blank"&gt;https://www.utasker.com/kinetis/compilers.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It is also possible to program the FRDM boards simply by dragging and dropping binary files onto the external hard drive that appears when their USB is connected.&lt;BR /&gt;There are various binaries and a boot loader for your board at these links that can be used:&lt;BR /&gt;- &lt;A href="https://www.utasker.com/kinetis/FRDM-KE02Z.html" target="_blank"&gt;https://www.utasker.com/kinetis/FRDM-KE02Z.html&lt;/A&gt;&lt;BR /&gt;- &lt;A href="https://www.utasker.com/kinetis/FRDM-KE02Z40M.html" target="_blank"&gt;https://www.utasker.com/kinetis/FRDM-KE02Z40M.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;You can also use the uTasker FRDM-KE02Z40M simulator to write, test and debug code for the processor/board before it arrives and then you can drop it onto the HW to see it running physically.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 21:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176097#M58689</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-10-30T21:13:43Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE02Z40M and CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176835#M58705</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As Mark already mentioned, CodeWarrior is an old IDE. Instead, I would recommend you use MCUXpresso IDE, which unlike CodeWarrior, it's completely free.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE" target="_self"&gt;Link to the MCUXpresso IDE webpage.&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Victor&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct"button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/P&gt;
&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 22:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z40M-and-CodeWarrior/m-p/1176835#M58705</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-11-02T22:31:46Z</dc:date>
    </item>
  </channel>
</rss>