<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KEA8 erase in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164673#M58397</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Sorry, not.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try to put the reset pin to low in order to try to start to debug it, I do not remember if the Multilink FX can provide the power to the board, I believe with this option will be easier. But I only use the Jlink&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 08 Oct 2020 17:19:03 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2020-10-08T17:19:03Z</dc:date>
    <item>
      <title>KEA8 erase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1163500#M58375</link>
      <description>&lt;P&gt;HI there,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been working with KEA8 (TSSOP 16 pins) + CW11 + MultiLink FX.&lt;/P&gt;&lt;P&gt;After debbug I decided to use&amp;nbsp;&lt;/P&gt;&lt;P&gt;SIM_SOPT =0x00000000;&lt;/P&gt;&lt;P&gt;In order to use alternate PTA4 and PAT0 functions. Now I want to erase some devices but I cannot do it.&lt;/P&gt;&lt;P&gt;Using flash to file option and then erase whole device, using KEAZN8M4.xml flash configuration.&lt;/P&gt;&lt;P&gt;Following errors appears&lt;/P&gt;&lt;P&gt;Error executing task KEAZN8M4. Wrong expression ${ProjDirPath}/Project_Settings/Debugger/init_kinetis.tcl; Could not expand variable ProjDirPath&lt;/P&gt;&lt;P&gt;If I use debug option there is no change to connect to device, is there any workaround?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 09:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1163500#M58375</guid>
      <dc:creator>Cram</dc:creator>
      <dc:date>2020-10-07T09:24:00Z</dc:date>
    </item>
    <item>
      <title>Re: KEA8 erase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164008#M58380</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/RSTPE-cleared-at-power-on-no-debugger/m-p/474436" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/RSTPE-cleared-at-power-on-no-debugger/m-p/474436&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a good day&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 15:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164008#M58380</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-10-07T15:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: KEA8 erase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164347#M58392</link>
      <description>&lt;P&gt;Hi vincent,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We do not have a Jlink from segger available, we mainly use pemicro tools.&lt;/P&gt;&lt;P&gt;I am using multilink universal FX. Is there any workaround?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 07:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164347#M58392</guid>
      <dc:creator>Cram</dc:creator>
      <dc:date>2020-10-08T07:46:44Z</dc:date>
    </item>
    <item>
      <title>Re: KEA8 erase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164673#M58397</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Sorry, not.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try to put the reset pin to low in order to try to start to debug it, I do not remember if the Multilink FX can provide the power to the board, I believe with this option will be easier. But I only use the Jlink&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 17:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-erase/m-p/1164673#M58397</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-10-08T17:19:03Z</dc:date>
    </item>
  </channel>
</rss>