<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL25Z unabled to debug. Programmed flash is protected and can't be read out. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-unabled-to-debug-Programmed-flash-is-protected-and-can-t/m-p/1163653#M58378</link>
    <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please attempt to connect it to MCUXpresso and use the flash tool to do a mass erase.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if you are able to connect it or not to MCUXpresso IDE to do the mass erase.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may also refer to the following document for more details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/" target="_self"&gt;Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Oct 2020 00:21:26 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2020-10-07T00:21:26Z</dc:date>
    <item>
      <title>KL25Z unabled to debug. Programmed flash is protected and can't be read out.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-unabled-to-debug-Programmed-flash-is-protected-and-can-t/m-p/1163105#M58371</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm using the KL25Z board for the first time so when I tried to debugg my code using the J-link Segger I get the following mesage: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For debugger connection the device needs to be unsecured.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&amp;nbsp;&lt;/SPAN&gt;If 'Do not show this message again' is selected, mass erase will be performed automatically in the future."&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;When I clicked "Yes" produces the further message: Failed to resume target process. Not allowed to access registers while running.&lt;/P&gt;&lt;P&gt;How can I solve this problem??&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 21:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-unabled-to-debug-Programmed-flash-is-protected-and-can-t/m-p/1163105#M58371</guid>
      <dc:creator>Raul_CN</dc:creator>
      <dc:date>2020-10-05T21:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z unabled to debug. Programmed flash is protected and can't be read out.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-unabled-to-debug-Programmed-flash-is-protected-and-can-t/m-p/1163653#M58378</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please attempt to connect it to MCUXpresso and use the flash tool to do a mass erase.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if you are able to connect it or not to MCUXpresso IDE to do the mass erase.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may also refer to the following document for more details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/" target="_self"&gt;Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 00:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-unabled-to-debug-Programmed-flash-is-protected-and-can-t/m-p/1163653#M58378</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-10-07T00:21:26Z</dc:date>
    </item>
  </channel>
</rss>