<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K22F - Ef(49) error.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22F-Ef-49-error/m-p/1162946#M58369</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147278"&gt;@can_pouliquen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could it be that you have updates that are waiting to install in your system?&amp;nbsp;&amp;nbsp;I find that when Windows is waiting on an update it causes all sorts of unrelated mayhem, especially with IO.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have you tried disconnecting your FRDM-K22F, closing MCUXpresso IDE and then doing any pending updates?&amp;nbsp; Even power cycling your PC could be helpful.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good luck!&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;</description>
    <pubDate>Mon, 05 Oct 2020 13:31:21 GMT</pubDate>
    <dc:creator>myke_predko</dc:creator>
    <dc:date>2020-10-05T13:31:21Z</dc:date>
    <item>
      <title>K22F - Ef(49) error.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22F-Ef-49-error/m-p/1162802#M58368</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently started working on a FRDM-K22F and started an empty project from scratch.&lt;/P&gt;&lt;P&gt;I configured the MCU settings according to the example projects of the SDK.&lt;/P&gt;&lt;P&gt;Everything went well for a few hours, the project was building and debugging normally. But the next morning, debugging wasn't functionning anymore, neither for my own project nor even for the SDK's example projects ! The green led indicating connexion with the debugger isn't lighting up (D1 led).&lt;/P&gt;&lt;P&gt;I keep having following error whenever I want to debug :&lt;/P&gt;&lt;P&gt;"EraseSector (0x800, 0x0, 0x1) status 0x1 - driver reported driver error - INTKFMM driver rc 16 - Flash protection violation&lt;BR /&gt;Sectors written: 1, unchanged: 1, total: 2&lt;BR /&gt;Closing flash driver FTFA_2K.cfx&lt;BR /&gt;Target error from Commit Flash write: Ef(49): Flash driver operation gave error."&lt;/P&gt;&lt;P&gt;I have already tried mass erasing the Flash or resurrecting a locked device, but nothing did the trick. I really have no idea where the problem could be comming from as, once again, everything was behaving properly just the day before.&lt;/P&gt;&lt;P&gt;If you have any idea on how to solve the problem, I would gladly welcome any help. Thank you in advance !&lt;/P&gt;&lt;P&gt;Here are the MCU settings I set up :&lt;/P&gt;&lt;P&gt;Flash driver : FTFA_2K.cfx&lt;/P&gt;&lt;P&gt;Flash location : 0x0 - size : 0x80000&lt;/P&gt;&lt;P&gt;Upper RAM location : 0x20000000 - size : 0x10000&lt;/P&gt;&lt;P&gt;Lower RAM location : 0x1fff0000 - size : 0x10000&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 08:30:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22F-Ef-49-error/m-p/1162802#M58368</guid>
      <dc:creator>can_pouliquen</dc:creator>
      <dc:date>2020-10-05T08:30:03Z</dc:date>
    </item>
    <item>
      <title>Re: K22F - Ef(49) error.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22F-Ef-49-error/m-p/1162946#M58369</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147278"&gt;@can_pouliquen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could it be that you have updates that are waiting to install in your system?&amp;nbsp;&amp;nbsp;I find that when Windows is waiting on an update it causes all sorts of unrelated mayhem, especially with IO.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have you tried disconnecting your FRDM-K22F, closing MCUXpresso IDE and then doing any pending updates?&amp;nbsp; Even power cycling your PC could be helpful.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good luck!&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 13:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22F-Ef-49-error/m-p/1162946#M58369</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2020-10-05T13:31:21Z</dc:date>
    </item>
  </channel>
</rss>