<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Setup for K81's USB Interface in MCUXpresso</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162503#M58361</link>
    <description>&lt;P&gt;Hi Hal&lt;/P&gt;&lt;P&gt;I don't use the config tools so I don't know what they support and what is missing.&lt;/P&gt;&lt;P&gt;Maybe you could add the missing configuration manually?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;</description>
    <pubDate>Fri, 02 Oct 2020 20:21:10 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2020-10-02T20:21:10Z</dc:date>
    <item>
      <title>Setup for K81's USB Interface in MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162364#M58358</link>
      <description>&lt;P&gt;&lt;U&gt;Clocking USB Interface:&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;(I also opened an NXP support case - # 00310003 - for this question.)&lt;/U&gt;&lt;/P&gt;&lt;P&gt;I'm trying to setup a Kinetis K81 (MK81FN256VDC15) in a "crystal-less" mode; i.e. to use the K81's internal 48MHz oscillator to be the source clock for all of the IC's clocking (no crystal on EXTAL0/XTAL0 pins). I can do most of this setup in MCUXpresso's Clock Config Tool. But for the IC's USB interface, I can't find how to access the USB interface related registers to set IRC_EN and CLOCK_RECOVER_EN which apparently is required to use this 48MHz internal clock as the USB FS clock. I don't see any USB support under the Peripherals Config Tool.&lt;/P&gt;&lt;P&gt;I'm using MCUXpressoIDE 11.2.0_4120 and SDK_2.5_TWR-K81F150M.zip. I'm targeting a K81 on a board of my own design but using the SDK for the TWR-K81 as a starting point.&lt;/P&gt;&lt;P&gt;&lt;U&gt;Powering the K81’s USB Interface using system power&lt;/U&gt;&lt;/P&gt;&lt;P&gt;In addition to setting up the clocking, I have a question about powering the K81’s USB interface.&amp;nbsp; The examples in the K81 datasheet and the demo/eval boards use bus-power to provide power to the K81’s VREGIN pin so show how to hookup VREGIN and VOUT33 to VBUS for that case.&amp;nbsp; My design is system-powered and the datasheet doesn’t explicitly provide guidance for that case. I’ve hooked up the VREGIN and VOUT33 pins to GND through 10Kohm resistor.&amp;nbsp; Is this correct or do I need to hookup VREGIN to my board’s 3.3V power supply (the supply powering the K81’s VBAT, VDD1-3, VDDA, and VDDIO_E pins) and add bypass caps on VREGIN and VOUT33?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 16:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162364#M58358</guid>
      <dc:creator>halsteger</dc:creator>
      <dc:date>2020-10-02T16:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: Setup for K81's USB Interface in MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162386#M58359</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;You can use the FRDM-K82F board as HW reference for connecting the VREGIN to a local power supply. The internal regulator is a linear one at about 0.6V drop-out and passes through when the input voltage is less than about 3.6V. Normally it is used with 5V input to have 3.3..3.6V output but will accept inputs down to 2.7V, with 2.1V output. &lt;EM&gt;It is worth checking that the USB transceivers still work well at low levels but 3V3 input is foreseen for such operation too.&lt;/EM&gt;&lt;BR /&gt;Pulling the input/output to GND will disable the regulator to save power but &lt;U&gt;will not allow the USB interface to operate&lt;/U&gt; since its transceiver will be disabled too.&lt;/P&gt;&lt;P&gt;The uTasker project also supports your device and USB in case you would like to look at an alternative solution which allows simulating the chip and the USB peripheral operation, as well as crystal-less USB mode. Applications are then automatically compatible with faster i.MX RT devices in case a switch is required later without extra firmware redevelopment effort, or benefit from lower price/better performance - eg.600MHz i.MX RT 1020 with 2 HS USB costs $2.30 against the K80 with single FS USB at $4.35. The uTasker K8x loader also gives secure, fail-safe field updating for applications from any source.&lt;/P&gt;&lt;P&gt;You probably are fully aware already but only use device mode of operation (not host) is possible without a crystal source.&lt;BR /&gt;In any case, the code that you seem to be missing is the following:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;SIM_SOPT2 |= (SIM_SOPT2_USBSRC | SIM_SOPT2_PLLFLLSEL_IRC48M); // set the source to IRC48M&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;SIM_CLKDIV2 = SIM_CLKDIV2_USBDIV_1; // no divide when IRC48M is used&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;USB_CLK_RECOVER_IRC_EN = USB_CLK_RECOVER_IRC_EN_IRC_EN; // enable 48MHz IRC clock and clock recovery&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;USB_CLK_RECOVER_CTRL = USB_CLK_RECOVER_CTRL_CLOCK_RECOVER_EN;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.utasker.com/kinetis/FRDM-K82F.html" target="_blank" rel="noopener"&gt;https://www.utasker.com/kinetis/FRDM-K82F.html&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.utasker.com/kinetis/TWR-K80F150M.html" target="_blank" rel="noopener"&gt;https://www.utasker.com/kinetis/TWR-K80F150M.html&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.utasker.com/iMX/RT1020.html" target="_blank" rel="noopener"&gt;https://www.utasker.com/iMX/RT1020.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 17:09:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162386#M58359</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-10-02T17:09:10Z</dc:date>
    </item>
    <item>
      <title>Re: Setup for K81's USB Interface in MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162458#M58360</link>
      <description>&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;I appreciate your quick and detailed reply.&lt;/P&gt;&lt;P&gt;Regarding the K81's USB power supply, it's looking like I need to supply power to VREGIN and add some bypass caps to GND on VREGIN and VOUT33. Thanks.&lt;/P&gt;&lt;P&gt;Regarding selecting the K81's internal 48KHz clock as the USB FS clock, I'm aware of the settings you describe but I can't find where in MCUXpresso I can make those register settings.&amp;nbsp; As I wrote, I can do most of the clock settings/selections using MCUXpresso's Clock Config Tool. But I can't find where I can set IRC_EN and CLOCK_RECOVER_EN. The USB interface doesn't appear in the Peripherals Config Tool (or any of the other Config Tools for that matter).&lt;/P&gt;&lt;P&gt;Hal&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 18:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162458#M58360</guid>
      <dc:creator>halsteger</dc:creator>
      <dc:date>2020-10-02T18:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: Setup for K81's USB Interface in MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162503#M58361</link>
      <description>&lt;P&gt;Hi Hal&lt;/P&gt;&lt;P&gt;I don't use the config tools so I don't know what they support and what is missing.&lt;/P&gt;&lt;P&gt;Maybe you could add the missing configuration manually?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 20:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1162503#M58361</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-10-02T20:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: Setup for K81's USB Interface in MCUXpresso</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1166173#M58451</link>
      <description>&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;Thanks again for your help with this issue.&lt;/P&gt;&lt;P&gt;Regarding the clocking issue, I was able to make some code modifications in addition to change some setting using the Clock Config Tool.&amp;nbsp; While I still don't understand why the USB interface doesn't appear as a peripheral under Peripherals Config Tool, I did get the design working.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding the USB Power and REGIN/VOUT33, I've hooked a 3V3 supply rail on the board up to REGIN and added some bypass caps on REGIN and VOUT33.&amp;nbsp; The interface is working properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;Hal&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 15:12:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setup-for-K81-s-USB-Interface-in-MCUXpresso/m-p/1166173#M58451</guid>
      <dc:creator>halsteger</dc:creator>
      <dc:date>2020-10-12T15:12:23Z</dc:date>
    </item>
  </channel>
</rss>