<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K64 with DS18B20 setting negative low temperature threshold in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1161486#M58328</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/157787"&gt;@mignacio&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&lt;/P&gt;
&lt;P&gt;This product is not part of the NXP portfolio. I am not sure what you are doing with the FRDM-K64 or how you are connecting these products.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2020 18:18:29 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2020-09-30T18:18:29Z</dc:date>
    <item>
      <title>FRDM-K64 with DS18B20 setting negative low temperature threshold</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1160269#M58293</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Has anyone set the DS18B20 low temperature threshold (do a Write Scratchpad 4Eh command) to &amp;lt; 0 C? e.g. -20C for example.&lt;/P&gt;&lt;P&gt;The problem I'm seeing is if I set the low threshold to negative value, while the high threshold to be positive, when I read back (Read Scratchpad BEh), the high threshold just becomes "-1".&amp;nbsp; &amp;nbsp; However if I write low threshold as 0 C and above positive number, the high threshold reads exactly the correct value I set before the read.&lt;/P&gt;&lt;P&gt;Comments?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;MI&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2020 20:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1160269#M58293</guid>
      <dc:creator>mignacio</dc:creator>
      <dc:date>2020-09-28T20:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64 with DS18B20 setting negative low temperature threshold</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1160891#M58313</link>
      <description>&lt;P&gt;Just example of setting TH, TL, config and then read back after write to scratchpad.&amp;nbsp; &amp;nbsp;High Threshold wrong -1C value when Low Threshold temp set to -20 before read.&amp;nbsp; &amp;nbsp;High threshold set to +50 C / +122 F but read back as -1C.&amp;nbsp; If TL set to -1 C, TH reads back as 0 C.&amp;nbsp; &amp;nbsp;Disproportional error.&amp;nbsp; (NOTE: "factory default" from waterproof device is TL = 70C, TH = 75C, small range.)&amp;nbsp; What you see here is what's read back after answering "Y" &amp;amp; "S" to prompt.&lt;/P&gt;&lt;P&gt;[2020-09-28 10:16:45.194] Change the high and low temperature thresholds (Y/N)? y&lt;BR /&gt;[2020-09-28 10:16:47.275]&lt;BR /&gt;[2020-09-28 10:16:47.275] Change to factory default (D) or specified thresholds (S)? s&lt;BR /&gt;[2020-09-28 10:16:48.108]&lt;BR /&gt;[2020-09-28 10:16:56.882] DS18B20 configuration register = 01111111&lt;BR /&gt;[2020-09-28 10:16:58.804]&lt;BR /&gt;[2020-09-28 10:17:05.903] DS18B20 Low threshold temperature = 11101100 Celsius = -20 C Farenheit = -4 F&lt;BR /&gt;[2020-09-28 10:17:36.127]&lt;BR /&gt;[2020-09-28 10:18:52.019] DS18B20 High threshold temperature = 11111111 Celsius = -1 C Farenheit = 31 F&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 19:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1160891#M58313</guid>
      <dc:creator>mignacio</dc:creator>
      <dc:date>2020-09-29T19:14:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64 with DS18B20 setting negative low temperature threshold</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1161486#M58328</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/157787"&gt;@mignacio&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&lt;/P&gt;
&lt;P&gt;This product is not part of the NXP portfolio. I am not sure what you are doing with the FRDM-K64 or how you are connecting these products.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 18:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-with-DS18B20-setting-negative-low-temperature-threshold/m-p/1161486#M58328</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2020-09-30T18:18:29Z</dc:date>
    </item>
  </channel>
</rss>