<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックmk10 UART modbus</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk10-UART-modbus/m-p/240377#M5820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN lang="NO-BOK"&gt;&lt;/SPAN&gt;My goal is to get an modbus Server running with an RS485 Uart on a MK10FN1M0VLQ12. So far I haven't found a suitable driver or newb example to get started on the low level stuff. Any Ideas for where to find Driver example for mk10?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I where to setup this from scratch and I want to set the pheripheral driver to handle silent interval max and min in characters (1 ch = 10 bit with stop bit) and clear to send intervall. &lt;/P&gt;&lt;P&gt;silent intervall &lt;/P&gt;&lt;P&gt;- If there is an space inbetween &amp;gt;1,5ch(min) and &amp;lt;3,5ch(max) the serial driver shall discard the incomming buffer. &lt;/P&gt;&lt;P&gt;- If the silent space is &amp;gt;3,5ch the incomming buffer shall be handled by the modbus rtu driver. &lt;/P&gt;&lt;P&gt;- If silent space is &amp;gt;4,5 outgoing buffer can be sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the proper solution, timer baud polled IO and/or with interrupt and/ with DMA?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 May 2013 19:33:02 GMT</pubDate>
    <dc:creator>mrandreas</dc:creator>
    <dc:date>2013-05-15T19:33:02Z</dc:date>
    <item>
      <title>mk10 UART modbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk10-UART-modbus/m-p/240377#M5820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN lang="NO-BOK"&gt;&lt;/SPAN&gt;My goal is to get an modbus Server running with an RS485 Uart on a MK10FN1M0VLQ12. So far I haven't found a suitable driver or newb example to get started on the low level stuff. Any Ideas for where to find Driver example for mk10?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I where to setup this from scratch and I want to set the pheripheral driver to handle silent interval max and min in characters (1 ch = 10 bit with stop bit) and clear to send intervall. &lt;/P&gt;&lt;P&gt;silent intervall &lt;/P&gt;&lt;P&gt;- If there is an space inbetween &amp;gt;1,5ch(min) and &amp;lt;3,5ch(max) the serial driver shall discard the incomming buffer. &lt;/P&gt;&lt;P&gt;- If the silent space is &amp;gt;3,5ch the incomming buffer shall be handled by the modbus rtu driver. &lt;/P&gt;&lt;P&gt;- If silent space is &amp;gt;4,5 outgoing buffer can be sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the proper solution, timer baud polled IO and/or with interrupt and/ with DMA?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2013 19:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk10-UART-modbus/m-p/240377#M5820</guid>
      <dc:creator>mrandreas</dc:creator>
      <dc:date>2013-05-15T19:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: mk10 UART modbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk10-UART-modbus/m-p/240378#M5821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although we don't offer a free library to implement Modbus, there are third party options, I suggest you check the following thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/308287"&gt;Is there any library for modbus?&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 13:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk10-UART-modbus/m-p/240378#M5821</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-07-02T13:57:01Z</dc:date>
    </item>
  </channel>
</rss>