<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetis K61 DDR_CKE pull-down</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079707#M57494</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Consider the following scenario:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;...&lt;/LI&gt;&lt;LI&gt;Application code is executed from the lower half of the DDR2 memory.&lt;/LI&gt;&lt;LI&gt;At some point&amp;nbsp;in-application programming is executed and&amp;nbsp;a&amp;nbsp;new application is loaded into the upper half of the DDR2 memory.&lt;/LI&gt;&lt;LI&gt;DDR2 memory is put into the self refresh mode and&amp;nbsp;MCU&amp;nbsp;is&amp;nbsp;reset (reset is needed to initialize&amp;nbsp;the core and the used peripherals to a known state).&lt;/LI&gt;&lt;LI&gt;DDR2 controller is initialized and control is passed to the application in the upper half of the DDR2 memory.&lt;/LI&gt;&lt;LI&gt;...&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the external pull-down resistor on the DDR_CKE&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;necessary&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;to keep the DDR2 memory in self-refresh mode&lt;SPAN&gt;&amp;nbsp;in this case after MCU is reset&lt;/SPAN&gt;? What might happen if there is no&amp;nbsp;pull-down?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case it matters MCU is MK61FX512VMJ12 and DDR2 memory is&amp;nbsp;MT47H128M16RT-25E-IT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yuri Panin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2020 17:44:46 GMT</pubDate>
    <dc:creator>panin</dc:creator>
    <dc:date>2020-05-12T17:44:46Z</dc:date>
    <item>
      <title>Kinetis K61 DDR_CKE pull-down</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079707#M57494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Consider the following scenario:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;...&lt;/LI&gt;&lt;LI&gt;Application code is executed from the lower half of the DDR2 memory.&lt;/LI&gt;&lt;LI&gt;At some point&amp;nbsp;in-application programming is executed and&amp;nbsp;a&amp;nbsp;new application is loaded into the upper half of the DDR2 memory.&lt;/LI&gt;&lt;LI&gt;DDR2 memory is put into the self refresh mode and&amp;nbsp;MCU&amp;nbsp;is&amp;nbsp;reset (reset is needed to initialize&amp;nbsp;the core and the used peripherals to a known state).&lt;/LI&gt;&lt;LI&gt;DDR2 controller is initialized and control is passed to the application in the upper half of the DDR2 memory.&lt;/LI&gt;&lt;LI&gt;...&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the external pull-down resistor on the DDR_CKE&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;necessary&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;to keep the DDR2 memory in self-refresh mode&lt;SPAN&gt;&amp;nbsp;in this case after MCU is reset&lt;/SPAN&gt;? What might happen if there is no&amp;nbsp;pull-down?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case it matters MCU is MK61FX512VMJ12 and DDR2 memory is&amp;nbsp;MT47H128M16RT-25E-IT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yuri Panin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 17:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079707#M57494</guid>
      <dc:creator>panin</dc:creator>
      <dc:date>2020-05-12T17:44:46Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K61 DDR_CKE pull-down</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079708#M57495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;Yes, I think an external 10k pull-down resistor is needed. The DDR_CKE pin of K61's default state is DISABLED. That is a high-impedance state. The TWR-K70 board also has this pull-down resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 06:27:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079708#M57495</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-05-15T06:27:08Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K61 DDR_CKE pull-down</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079709#M57496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just as I suspected. Thank you very much, Jing!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yuri Panin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 May 2020 07:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K61-DDR-CKE-pull-down/m-p/1079709#M57496</guid>
      <dc:creator>panin</dc:creator>
      <dc:date>2020-05-16T07:59:13Z</dc:date>
    </item>
  </channel>
</rss>