<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK02 external clock</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078663#M57464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;BR /&gt;In a custom project we use MK02FN64VLF10 to generate low frequency sinusoidal waveform.&lt;BR /&gt;We need stability and precision for those waveform, so we don't use IRC clock, but external 8MHz clock generator instead.&lt;BR /&gt;Now, for a design review we need to reduce current consumption of board, and we use crystal oscillator... and here is the issue.&lt;BR /&gt;The MK02FN64VLF10 boots with IRC clock correctly, but internal oscillator with external crystal don't start, so we cannot switch system clock to oscillator source.&lt;BR /&gt;Can you help me?&lt;/P&gt;&lt;P&gt;Thank to all&lt;BR /&gt;Massimo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jun 2020 15:11:48 GMT</pubDate>
    <dc:creator>massimopiazzabw</dc:creator>
    <dc:date>2020-06-09T15:11:48Z</dc:date>
    <item>
      <title>MK02 external clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078663#M57464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;BR /&gt;In a custom project we use MK02FN64VLF10 to generate low frequency sinusoidal waveform.&lt;BR /&gt;We need stability and precision for those waveform, so we don't use IRC clock, but external 8MHz clock generator instead.&lt;BR /&gt;Now, for a design review we need to reduce current consumption of board, and we use crystal oscillator... and here is the issue.&lt;BR /&gt;The MK02FN64VLF10 boots with IRC clock correctly, but internal oscillator with external crystal don't start, so we cannot switch system clock to oscillator source.&lt;BR /&gt;Can you help me?&lt;/P&gt;&lt;P&gt;Thank to all&lt;BR /&gt;Massimo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2020 15:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078663#M57464</guid>
      <dc:creator>massimopiazzabw</dc:creator>
      <dc:date>2020-06-09T15:11:48Z</dc:date>
    </item>
    <item>
      <title>Re: MK02 external clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078664#M57465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Massimo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Usually, this is due to the capacitance in the crystal is not enough to stabilize the crystal, I'll suggest checking the following application &lt;A href="https://www.nxp.com/docs/en/application-note/AN3208.pdf"&gt;note.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 13:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078664#M57465</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-06-11T13:43:04Z</dc:date>
    </item>
    <item>
      <title>Re: MK02 external clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078665#M57466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the MCG register C2 there is a gain control. This must match with the crystal circuitry.&lt;/P&gt;&lt;P&gt;If the crystal is not loaded with caps and R use low gain mode. If it is loaded use high gain mode.&lt;/P&gt;&lt;P&gt;A mismatch will not allow the crystal oscillator to start up and is the most typical cause of the difficulty presently seen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 14:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-external-clock/m-p/1078665#M57466</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-06-11T14:39:13Z</dc:date>
    </item>
  </channel>
</rss>