<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cyclone FX error $00000007 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073431#M57360</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I asked the question to the P&amp;amp;E support but I think I can also ask the question here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the Cyclone Fx:&lt;/P&gt;&lt;P&gt;Version / Revision: Rev A - v10.13-2.3&lt;BR /&gt;Operating System: Windows 10 64-bit &lt;BR /&gt;Hello,&lt;BR /&gt;I'm using the Cyclone Fx universal since many years on any product, mainly with &lt;BR /&gt;NXP Kinetis microcontroller (K70, K60)&lt;BR /&gt;&lt;BR /&gt;Now we have a project based on &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;K02FN64M10&lt;/STRONG&gt;&lt;/SPAN&gt;. &lt;BR /&gt;But we have problem to program it with cyclone.&lt;BR /&gt;&lt;BR /&gt;-&amp;gt; Get a blank board&lt;BR /&gt;-&amp;gt; Flash with Cyclone FX universal (Press Start button) -&amp;gt; Succesfull&lt;BR /&gt;-&amp;gt; press again Start button -&amp;gt; Success.&lt;BR /&gt;-&amp;gt; Switch off/On the board -&amp;gt; programmed software start properly&lt;BR /&gt;-&amp;gt; Press Start button -&amp;gt; Error $00000007&lt;BR /&gt;&lt;BR /&gt;So this can't come from wiring problem.&lt;BR /&gt;&lt;BR /&gt;The script is always the same than I used for K70 and K60:&lt;BR /&gt;CM - SS - EM - PM - VC - SD (Secure Device)&lt;BR /&gt;&lt;BR /&gt;About the Secure device, I always do it, then it was not problem because we &lt;BR /&gt;start sequence by an Erase Module (Or Erase If Not Blank)&lt;BR /&gt;&lt;BR /&gt;-&amp;gt; When I try now to connect with MCUExpresso and the MultiLink Universal to &lt;BR /&gt;debug, It ask to me the device is secured then I must Erase it. I press Ok to &lt;BR /&gt;do it. The same question is asked immedialty a second time, Then I press Ok. So &lt;BR /&gt;Now I get the "P&amp;amp;E Connection Assisant" Window&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't now why the controller is locked like that without possibility to do anything with Cyclone FX or USB multilink?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I use the McuExpresso with the SDK SDK_2.x_MK02FN64xxx10 version v2.7.0. During devellopement I always use the compiler option "Debug". To generate file to insert into the Cyclone, I use the "Release" compilation option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2020 14:06:11 GMT</pubDate>
    <dc:creator>arnogir</dc:creator>
    <dc:date>2020-07-21T14:06:11Z</dc:date>
    <item>
      <title>Cyclone FX error $00000007</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073431#M57360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I asked the question to the P&amp;amp;E support but I think I can also ask the question here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the Cyclone Fx:&lt;/P&gt;&lt;P&gt;Version / Revision: Rev A - v10.13-2.3&lt;BR /&gt;Operating System: Windows 10 64-bit &lt;BR /&gt;Hello,&lt;BR /&gt;I'm using the Cyclone Fx universal since many years on any product, mainly with &lt;BR /&gt;NXP Kinetis microcontroller (K70, K60)&lt;BR /&gt;&lt;BR /&gt;Now we have a project based on &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;K02FN64M10&lt;/STRONG&gt;&lt;/SPAN&gt;. &lt;BR /&gt;But we have problem to program it with cyclone.&lt;BR /&gt;&lt;BR /&gt;-&amp;gt; Get a blank board&lt;BR /&gt;-&amp;gt; Flash with Cyclone FX universal (Press Start button) -&amp;gt; Succesfull&lt;BR /&gt;-&amp;gt; press again Start button -&amp;gt; Success.&lt;BR /&gt;-&amp;gt; Switch off/On the board -&amp;gt; programmed software start properly&lt;BR /&gt;-&amp;gt; Press Start button -&amp;gt; Error $00000007&lt;BR /&gt;&lt;BR /&gt;So this can't come from wiring problem.&lt;BR /&gt;&lt;BR /&gt;The script is always the same than I used for K70 and K60:&lt;BR /&gt;CM - SS - EM - PM - VC - SD (Secure Device)&lt;BR /&gt;&lt;BR /&gt;About the Secure device, I always do it, then it was not problem because we &lt;BR /&gt;start sequence by an Erase Module (Or Erase If Not Blank)&lt;BR /&gt;&lt;BR /&gt;-&amp;gt; When I try now to connect with MCUExpresso and the MultiLink Universal to &lt;BR /&gt;debug, It ask to me the device is secured then I must Erase it. I press Ok to &lt;BR /&gt;do it. The same question is asked immedialty a second time, Then I press Ok. So &lt;BR /&gt;Now I get the "P&amp;amp;E Connection Assisant" Window&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't now why the controller is locked like that without possibility to do anything with Cyclone FX or USB multilink?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I use the McuExpresso with the SDK SDK_2.x_MK02FN64xxx10 version v2.7.0. During devellopement I always use the compiler option "Debug". To generate file to insert into the Cyclone, I use the "Release" compilation option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 14:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073431#M57360</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2020-07-21T14:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: Cyclone FX error $00000007</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073432#M57361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arnaud, I hope you're doing well!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just to confirm, are you using a custom board?&lt;/P&gt;&lt;P&gt;If so, could you please confirm if the connections were done properly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 22:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073432#M57361</guid>
      <dc:creator>Sebastian_Del_Rio</dc:creator>
      <dc:date>2020-07-23T22:05:45Z</dc:date>
    </item>
    <item>
      <title>Re: Cyclone FX error $00000007</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073433#M57362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes it is a custom board.&lt;/P&gt;&lt;P&gt;We devellop it by the begining of this year.&lt;/P&gt;&lt;P&gt;We made all the software devellopment without any problem with MCUExpresso and P&amp;amp;E Multilink universal.&lt;/P&gt;&lt;P&gt;Then now, to deliver the first two prototype to our customer, we use our mass production tool: Cyclone FX.&lt;/P&gt;&lt;P&gt;(Like many other product based on kinetis)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first Cyclone FX programmtion was Ok, but I need to update the software of this board (flash from v1.0.0 to to v1.0.1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is at this time I seen I can't flash it again with error $00000007, then the MultiLink universal cans't access also.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 05:38:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073433#M57362</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2020-07-24T05:38:40Z</dc:date>
    </item>
    <item>
      <title>Re: Cyclone FX error $00000007</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073434#M57363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I just made change the processor on my board.&lt;BR /&gt;Then I connect well with USB Multilink Universal.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Then I flash with Cyclone FX but without option "SD" = Secure device.&lt;BR /&gt;All it OK, flash is Ok and the application start, even after a power off/on cycle.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I can flash board again and many time without problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I flash image &lt;STRONG&gt;with&lt;/STRONG&gt; "SD" option. I can flash it many time if I not restart the processor. But after a power off/on cycle, flash is impossible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This indicate the "SD" option is the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 10:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073434#M57363</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2020-07-24T10:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Cyclone FX error $00000007</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073435#M57364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Thanks to the P&amp;amp;E support, it said to me the Unsecure Device need Hardwar Reset.&lt;/P&gt;&lt;P&gt;Our schematic link JRAG RST signal to the PTA5 (JTAG_RST in ALT7 only... not default...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I linked the JTAG RST signal to the Hardware µC Reset Pin 34 and all work properly now&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2020 08:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cyclone-FX-error-00000007/m-p/1073435#M57364</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2020-07-28T08:20:00Z</dc:date>
    </item>
  </channel>
</rss>