<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What is the IO buffer propagation delay for K61 MCU? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-IO-buffer-propagation-delay-for-K61-MCU/m-p/1068830#M57249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am studying the write and read timing of the DDR controller including the timing of DDR signals through the DDR PHY interface. As far as I know, the read and write timing in PHY interface can be controlled through the DDR registers. However, I cannot justify the timing of the PHY interface with the missing piece of &lt;STRONG&gt;DDR&lt;/STRONG&gt;&amp;nbsp;&lt;STRONG&gt;IO buffer propagation delay&lt;/STRONG&gt; of the K61 MCU with part number of&amp;nbsp;MK61FN1M0VMJ15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, based on the datasheet for NXP IMX50 with the link to the datasheet below,&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf" title="https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf"&gt;https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DDR IO buffer propagation delay is given (pg 47),&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45899i7087746ABC0E8ED5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope that anyone of you guys can help to provide the IO buffer propagation delay of the K61 MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2020 13:52:13 GMT</pubDate>
    <dc:creator>sing-yew_chan</dc:creator>
    <dc:date>2020-04-22T13:52:13Z</dc:date>
    <item>
      <title>What is the IO buffer propagation delay for K61 MCU?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-IO-buffer-propagation-delay-for-K61-MCU/m-p/1068830#M57249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am studying the write and read timing of the DDR controller including the timing of DDR signals through the DDR PHY interface. As far as I know, the read and write timing in PHY interface can be controlled through the DDR registers. However, I cannot justify the timing of the PHY interface with the missing piece of &lt;STRONG&gt;DDR&lt;/STRONG&gt;&amp;nbsp;&lt;STRONG&gt;IO buffer propagation delay&lt;/STRONG&gt; of the K61 MCU with part number of&amp;nbsp;MK61FN1M0VMJ15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, based on the datasheet for NXP IMX50 with the link to the datasheet below,&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf" title="https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf"&gt;https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DDR IO buffer propagation delay is given (pg 47),&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45899i7087746ABC0E8ED5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope that anyone of you guys can help to provide the IO buffer propagation delay of the K61 MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 13:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-IO-buffer-propagation-delay-for-K61-MCU/m-p/1068830#M57249</guid>
      <dc:creator>sing-yew_chan</dc:creator>
      <dc:date>2020-04-22T13:52:13Z</dc:date>
    </item>
    <item>
      <title>Re: What is the IO buffer propagation delay for K61 MCU?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-IO-buffer-propagation-delay-for-K61-MCU/m-p/1068831#M57250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, we do not have the timing at that very detailed level. Instead, the &lt;A href="https://www.nxp.com/docs/en/data-sheet/K61P256M150SF3.pdf"&gt;datasheet&lt;/A&gt; contains the “output valid” specification which covers the timing specifications of the DDR controller in regards to the external signals.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2020 17:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-IO-buffer-propagation-delay-for-K61-MCU/m-p/1068831#M57250</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-04-24T17:00:50Z</dc:date>
    </item>
  </channel>
</rss>