<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Query regarding soft error handling as per IEC 61508 standard 2010 edition in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Query-regarding-soft-error-handling-as-per-IEC-61508-standard/m-p/1063190#M57142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Swapnil:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry I don't have any materials about MK60FX512VMD15 certification. IEC61508 applies to the Function Safety of a system. NXP does make microcontrollers that target functional safety, but not in the Kinetis range.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the MCUs that passed safety standards are listed here:&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fproduct-information%2Ffunctional-safety-for-iso-26262-and-iec-61508%3AFNCTNLSFTY%3Ffsrch%3D1%26sr%3D1%26pageNum%3D1" rel="nofollow" target="_blank"&gt;Functional Safety for ISO 26262 and IEC 61508|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will update if I have further information about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Apr 2020 03:54:53 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2020-04-09T03:54:53Z</dc:date>
    <item>
      <title>Query regarding soft error handling as per IEC 61508 standard 2010 edition</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Query-regarding-soft-error-handling-as-per-IEC-61508-standard/m-p/1063189#M57141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using kinetis K60 processor MK60FX512VMD15 in one of our product. We are using MQX RTOS version 4.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to take care of soft errors (bit flips caused due to radiations, cosmic rays etc..) that could occur&lt;BR /&gt;in the SRAM present on kinetis K60 processor. The requirement comes from IEC 61508 standard (2010) &lt;BR /&gt;edition which requires assessment of random hardware failures (Probability of Failure on Demand - PFD, safe failure fraction - SFF).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindnly let me know if there is any software based solution to take care of soft errors in SRAM on Kinetis K60.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not possible to handle through software, please suggest any other approach to satisfy the IEC 61508 &lt;BR /&gt;requirements related to soft error handling.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also kindly let me know Soft Error Rate (SER) for the SRAM present on MK60FX512VMD15 processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Warm Regards,&lt;BR /&gt;Swapnil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2020 06:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Query-regarding-soft-error-handling-as-per-IEC-61508-standard/m-p/1063189#M57141</guid>
      <dc:creator>swapnilv</dc:creator>
      <dc:date>2020-04-06T06:31:34Z</dc:date>
    </item>
    <item>
      <title>Re: Query regarding soft error handling as per IEC 61508 standard 2010 edition</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Query-regarding-soft-error-handling-as-per-IEC-61508-standard/m-p/1063190#M57142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Swapnil:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry I don't have any materials about MK60FX512VMD15 certification. IEC61508 applies to the Function Safety of a system. NXP does make microcontrollers that target functional safety, but not in the Kinetis range.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the MCUs that passed safety standards are listed here:&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fproduct-information%2Ffunctional-safety-for-iso-26262-and-iec-61508%3AFNCTNLSFTY%3Ffsrch%3D1%26sr%3D1%26pageNum%3D1" rel="nofollow" target="_blank"&gt;Functional Safety for ISO 26262 and IEC 61508|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will update if I have further information about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2020 03:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Query-regarding-soft-error-handling-as-per-IEC-61508-standard/m-p/1063190#M57142</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-04-09T03:54:53Z</dc:date>
    </item>
  </channel>
</rss>