<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-K60F120M doesn't work with TWR-SER2. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-doesn-t-work-with-TWR-SER2/m-p/239122#M5709</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using MQX try this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;enable HS driver &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;#define USBCFG_DEFAULT_DEVICE_CONTROLLER (&amp;amp;_bsp_usb_dev_ehci0_if)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define USBCFG_DEFAULT_HOST_CONTROLLER (&amp;amp;_bsp_usb_host_ehci0_if) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;And rebuild libraries.&lt;/P&gt;&lt;P&gt;This works on the TWR-K70 , try it on the TWR-K60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, In the USB stack, you need to setup HIGH_SPEED_DEVICE to 1 in user_config.h in each USB stack project you want to test with TWR-SER2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Sep 2013 17:46:12 GMT</pubDate>
    <dc:creator>hectorsanchez</dc:creator>
    <dc:date>2013-09-18T17:46:12Z</dc:date>
    <item>
      <title>TWR-K60F120M doesn't work with TWR-SER2.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-doesn-t-work-with-TWR-SER2/m-p/239121#M5708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am able to use the TWR-K60F120M with the TWR-SER, run the hid example, and get the mouse and keyboard to work just fine.&amp;nbsp; However I need to run high speed USB with the TWR-SER2.&amp;nbsp; I shunted J21 as instructed for high speed USB but it does not work.&amp;nbsp; I can't even run the application.&amp;nbsp; I tried changing BSP_USB_TWR_SER2 to 1 in twrk60f120m.h but that didn't help.&amp;nbsp; Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2013 14:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-doesn-t-work-with-TWR-SER2/m-p/239121#M5708</guid>
      <dc:creator>rogerdoak</dc:creator>
      <dc:date>2013-09-18T14:33:23Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M doesn't work with TWR-SER2.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-doesn-t-work-with-TWR-SER2/m-p/239122#M5709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using MQX try this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;enable HS driver &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;#define USBCFG_DEFAULT_DEVICE_CONTROLLER (&amp;amp;_bsp_usb_dev_ehci0_if)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define USBCFG_DEFAULT_HOST_CONTROLLER (&amp;amp;_bsp_usb_host_ehci0_if) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;And rebuild libraries.&lt;/P&gt;&lt;P&gt;This works on the TWR-K70 , try it on the TWR-K60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, In the USB stack, you need to setup HIGH_SPEED_DEVICE to 1 in user_config.h in each USB stack project you want to test with TWR-SER2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2013 17:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-doesn-t-work-with-TWR-SER2/m-p/239122#M5709</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2013-09-18T17:46:12Z</dc:date>
    </item>
  </channel>
</rss>