<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: ls1021a/ls1028a device tree (tsn)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ls1021a-ls1028a-device-tree-tsn/m-p/1060771#M57084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could refer to ls1021atsn dts file provided in OpenIL, please refer to the attached dts file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could refer to "Chapter 2 Getting started" in&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf" title="https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf"&gt;https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf&lt;/A&gt;&amp;nbsp;to download OpenIL and run the following command to get Linux Kernel source code in&amp;nbsp;output/build/linux-OpenIL-v1.7-linux-202001.&lt;/P&gt;&lt;P&gt;$&amp;nbsp;make nxp_ls1021atsn_defconfig&lt;/P&gt;&lt;P&gt;$ make linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then refer to&amp;nbsp;arch/arm/boot/dts/ls1021a-tsn.dts in Linux Kernel source code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Apr 2020 06:06:35 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2020-04-07T06:06:35Z</dc:date>
    <item>
      <title>ls1021a/ls1028a device tree (tsn)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ls1021a-ls1028a-device-tree-tsn/m-p/1060770#M57083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the device tree for the ls1028a where we are using SPI3 with an attacted &lt;SPAN class=""&gt;&lt;EM&gt;KSZ8567&lt;/EM&gt;&lt;/SPAN&gt; ethernet switch.&lt;/P&gt;&lt;P&gt;As I understand it, the ls1021a (tsn) variant is pretty similar to our custom-board in the sense that it also has an external ethernet switch. There, I downloaded the software for the ls1021a to lookat the device tree to get some ideas.. However, the package I downloaded did not contain any DTS-files. I cannot find it in the LSDK19.09 either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to share the device tree of ls1021a here, or point me in the right direction where I can find it? Hopefully, I can also understand which driver(s) to include in the kernel config..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Help is appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best rgds,&lt;/P&gt;&lt;P&gt;Tom Roar Pedersen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Apr 2020 17:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ls1021a-ls1028a-device-tree-tsn/m-p/1060770#M57083</guid>
      <dc:creator>trp</dc:creator>
      <dc:date>2020-04-04T17:24:22Z</dc:date>
    </item>
    <item>
      <title>Re: ls1021a/ls1028a device tree (tsn)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ls1021a-ls1028a-device-tree-tsn/m-p/1060771#M57084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could refer to ls1021atsn dts file provided in OpenIL, please refer to the attached dts file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could refer to "Chapter 2 Getting started" in&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf" title="https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf"&gt;https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf&lt;/A&gt;&amp;nbsp;to download OpenIL and run the following command to get Linux Kernel source code in&amp;nbsp;output/build/linux-OpenIL-v1.7-linux-202001.&lt;/P&gt;&lt;P&gt;$&amp;nbsp;make nxp_ls1021atsn_defconfig&lt;/P&gt;&lt;P&gt;$ make linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then refer to&amp;nbsp;arch/arm/boot/dts/ls1021a-tsn.dts in Linux Kernel source code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2020 06:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ls1021a-ls1028a-device-tree-tsn/m-p/1060771#M57084</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-04-07T06:06:35Z</dc:date>
    </item>
  </channel>
</rss>